Using the Hosted Storage Service

The benefits of a hosted storage implementation are the same a other hosted services from Schneider Electric. This includes a reduced cost of ownership where:

  • Schneider Electric maintains the hosted storage and maintaining high availability.

  • All the storage configurations are set up by Schneider Electric automatically when you filled out the Request a Tenant form.

  • You, as the customer, do not need to allocate hardware, maintain the operating system (security patches), install the Storage Service, or upgrade the Storage Service.

  • You also do not need to manage the IT security for an IIS service that needs to be able to communicate with external systems.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?