Configure Storage Service Options

The Storage Service is a holding tank that holds cached GIS data from different feature services.

Example: After the Edge Service pulls the feeder and its features, it packages the information into a Geodatabase Region Resource (GRR) file and uploads it to the storage service host. When an implementation, like Outage Management Systems (OMS), wants to consume the GRR file, they can contact the Storage Service and request a download.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?