Upgrading the On-Prem Storage Service

If your implementation uses an on-prem storage service, you first need to update to the latest version of the storage service. Perform the following steps to update from a prior installation of the storage service:
  1. Shut down the running storage service using Internet Information Services (IIS).
  2. Uninstall the old version of the storage service.
  3. Follow the instructions in Configuring the On-Prem Storage Service to complete a new installation.
  4. Restart the service using IIS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?