BQT6904800 -03

Control Symbols of VCB

Table 4 Rack-in/Rack-out Symbols

Description

Symbols

Manual operation instruction for rack-in/rack-out

Connected/service position

Disconnected/test position

Table 5 EvoPacT HVX VCB Symbols

Description

Symbols

Description

Symbols

ON push button

Spring discharged

OFF push button

Operating counter

Spring charged and ready-to-close indicator

Padlock for push button selector (optional feature)

VCB OFF

VCB ON

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?