BQT6904800 -03

Operating the CVX Contactor

Switching OFF via the Push Rod

Follow the below steps to switch OFF the CVX contactor via push rod:

  1. Take the push rod (2) from the transport trolley. Refer to Figure 42.

  2. Insert the push rod (2) through switch OFF guide (1) of the CVX contactor cubicle front door.

  3. Push the switch OFF button with the push rod (2).

    WARNING
    HAZARD OF INAPPROPRIATE OPERATION
    Ensure that the CVX contactor is switched OFF via push rod, and the position indicator indicates OFF.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  4. Remove the push rod from the switch OFF guide (1) of CVX contactor cubicle door.

  5. Place the push rod (2) back into the transport trolley.

Figure 42
Switching OFF the CVX Contactor via Push Rod

1

Switch OFF guide

2

Push rod

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?