BQT6904800 -03

Switching OFF the Contactor Cubicle E/S

Follow the below steps to switch ON the contactor cubicle E/S:

  1. Push the slider (2) upwards and insert the handle (1) to the E/S with the handle rod pointing to the right. Refer to the Figure 48.

  2. Turn the E/S handle (1) counter–clockwise by approximately 95°.

  3. Check position indicator (3). Make sure that the E/S is OFF.

  4. Remove the E/S handle (1) and place it back into the transport trolley.

Figure 48
Switching E/S OFF

1

Handle

3

Position indicator

2

Slider

   
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?