BQT6904800 -03

Access to the Contactor Cubicle Cable Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Before accessing the cable compartment, ensure the E/S is ON. Refer to Switching ON the Contactor Cubicle E/S.
Failure to follow these instructions will result in death or serious injury.

Additional cylinder locks can be installed to help secure both the cable compartment door and the switching device compartment door of the cubicle.

Removal of the Cable Compartment Door

Follow the below steps to open the cable compartment door:

  1. Lift and turn the cable compartment cover. Refer to Figure 67.

  2. Once the assembly is complete, gently lift the cable compartment door, turn it to the closed position, and lower it to close.


Figure 67
Removal of the Cable Compartment Door

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?