BQT6904800 -03

Feeder with Contactor Cubicle

Feeder with contactor cubicle are available with a maximum rated

voltage of 12 kV.

Figure 2
Feeder with Contactor (FC)

1

Voltage Detecting and Indicating System (VDIS) and PowerLogic Partial Discharge100 (PD100)

6

CT

2

Nameplate

7

Cables

3

Door of switching device compartment

8

Shutter actuation

4

Operator of the E/S

9

Truck-type vacuum contactor CVX with fuses

5

Cable compartment

10

Busbars

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?