BQT6904800 -03

Switching the VCB Manually

Switching ON via the Push Rod

The closed-door operation of the EvoPacT HVX VCB involves switching the VCB to the connected/service position or rack-in position.

Follow the below steps to switch ON VCB via push rod:

  1. Take the push rod (1) from the transport trolley. Refer to Figure 40.

  2. Insert the push rod (1) through switch ON guide (2) of the VCB front door.

  3. Push the switch ON button with the push rod (1).

    WARNING
    HAZARD OF INAPPROPRIATE OPERATION
    Ensure that the VCB is switched ON via push rod and the position indicator indicates ON.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

  4. Remove the push rod from the switch ON guide (2) of VCB door.

  5. Place the push rod (1) back into the transport trolley.

Figure 40
Switching ON the EvoPacT HVX VCB via Push Rod

1

Push rod

2

Switch ON guide

The energy-storing device can be charged again immediately after switching ON either by hand or by motor. If supply voltage is present, the energy-storing device is charged automatically.

Switching OFF via the Push Rod

Follow the below steps to switch OFF VCB via push rod:

  1. Take the push rod (1) from the transport trolley. Refer to Figure 41.

  2. Insert the push rod (1) through switch OFF guide (2) of the VCB front door.

  3. Push the switch OFF button with the push rod (1).

    WARNING
    HAZARD OF INAPPROPRIATE OPERATION
    Ensure that the VCB is switched OFF via push rod and the position indicator indicates OFF.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

  4. Remove the push rod from the switch OFF guide (2) of VCB door.

  5. Place the push rod (1) back into the transport trolley.

Figure 41
Switching OFF the EvoPacT HVX VCB via Push Rod

1

Push rod

2

Switch OFF guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?