BQT6904800 -03

Charging the VCB Energy Storing Device

Initial Position:

  • VCB: OFF

  • Energy storing device: Released

Motorized Charging

The energy-storing device automatically charges upon the application of the motor supply voltage.

The position indicator of the energy-storing device indicates the charged condition (4). Refer to Figure 39.

Manual Charging

Follow the below steps to charge the VCB:

  1. Rotate the knob (1) counter-clockwise to access the manual charging of the gear box (2). Refer to Figure 39.

  2. Insert the crank handle (3) into the guide (2).

  3. Turn the crank handle (3) clockwise, until complete charging of the mechanism.

    NOTE: Ensure that the direction indicator (4) shows that it is in charged condition.
  4. Remove and place the crank handle (3) back into the transport trolley.

Figure 39
Manual Charging of EvoPacT HVX VCB

1

Knob

3

Crank handle

2

Guide

4

Direction indicator (charged)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?