DOCA0265EN-07

Description

Introduction

The MicroLogic Active control unit includes:

  • LEDs to monitor the status of the circuit breaker.

  • A local Human Machine Interface comprising a graphic display with colored backlight, navigation buttons, and direct access buttons.

  • LEDs to monitor the cause of trips and alarms.

Control Unit Description

A MicroLogic Active type, indicated by the color of the head of the control unit:

  • Black head: MicroLogic Active A/E control unit without Zigbee wireless communication

  • Green head: MicroLogic Active AP/EP control unit with Zigbee wireless communication

B Trip information/test/reset button

C Trip cause LEDs

D Status LEDs:

  • Ready LED

  • Status bar

  • ERMS LED

E NFC wireless communication zone (not available with MicroLogic Active 6.0 Ei control unit)

F Graphic display screen

G Navigation buttons

H Protection settings button (under sealable cover)

I ERMS button (under sealable cover)

J QR code to access product information

K Control unit type and identification number

L USB-C port (under sealable cover)

M Internal battery drawer module

N Sensor plug with the rated current of the circuit breaker

O MicroLogic sealable transparent cover

Trip Information/Test/Reset Button

For information about the button, see Trip Information/Test/Reset Button.

Trip Cause LEDs

The indications of the trip cause LEDs depend on the type of MicroLogic Active control unit.

LEDs

Description

L

MicroLogic Active 2.0, 5.0, 6.0: Overload pre-alarm, the load exceeds 90% and is lower than 105% of the Ir setting of the long-time protection.

MicroLogic Active 2.0, 5.0, 6.0: Overload alarm, the load exceeds 105% of the Ir setting of the long-time protection.

MicroLogic Active 2.0, 5.0, 6.0: Trip due to long-time protection.

S

MicroLogic Active 5.0, 6.0: Trip due to short-time protection.

I

MicroLogic Active 2.0, 5.0, 6.0: Trip due to instantaneous protection.

G

MicroLogic Active 6.0: Trip due to ground-fault protection.

O

MicroLogic Active 2.0, 5.0, 6.0: Trip due to advanced and other, customized protection.

NOTE: If the MicroLogic Active control unit is not powered, the trip cause LEDs go off after 2 hours. After this period, press the button to light them again.

Status LEDs

LED

Description

Ready LED

The Ready LED flashes slowly under normal operation.

Status bar

The Status bar alerts the user to the health state of the circuit breaker:

  • Green Status bar: no action required.

  • Orange Status bar: medium severity alarm that requires non-urgent maintenance action.

  • Red Status bar: high severity alarm that requires immediate maintenance action.

ERMS LED

The ERMS (Energy Reduction Maintenance Setting) LED informs the user when ERMS is engaged, and ERMS protection settings are operational:

  • Blue LED: ERMS engaged

  • Off: ERMS disengaged

For more information, see the description of Local Indications.

NFC Communication Zone

The NFC communication zone is used to establish an NFC connection between a smartphone running the EcoStruxure Power Device app and the MicroLogic Active control unit. When the connection is established, the circuit breaker operating data is automatically uploaded to the smartphone.

NOTE: NFC communication is not available with MicroLogic Active 6.0 Ei control unit.

Display Screen with Navigation Buttons

The local HMI screen and buttons are used to:

  • Navigate the menu structure.

  • Display monitored values.

  • Access and edit configuration settings.

Protection Settings Button

The protection settings button is used to directly access the protection setting procedure.

ERMS Button

The ERMS button is used to directly engage and disengage the ERMS function.

QR Code

When the QR code on the front face of a MicroLogic Active control unit is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed. The landing page displays some information about the device, including traceability information, and a list of menus.

Control Unit Identification Number

The identification number PPPPPPYYWWDLNNNNLV9••••• is made up as follows:

  • The serial number of the MicroLogic Active control unit in the format PPPPPPYYWWDLNNNN, where the codes are defined as follows:

    • PPPPPP: Plant code

    • YY: Year (00 to 99), for example 24 for 2024

    • WW: Week of the year (01 to 53), for example 25

    • D: Day of the week, with 1 representing Monday and 7 representing Sunday, for example 5

      for Friday
    • L: Unique manufacturing line code or machine code within the plant

    • NNNN: Unique product number (0001 to 9999) generated on the day of manufacturing, by the plant manufacturing line or the plant machine

  • The commercial reference of the control unit in the format LV9•••••

Use the identification number to register your MicroLogic Active control unit through mySchneider app, the customer care mobile application.

Registering your MicroLogic Active control unit enables you to keep your records up to date and enables traceability.

Control Unit Type

The type of MicroLogic Active control unit is indicated by a number and one or two letters:

  • The number (for example, 6.0) defines the type of protection provided by the control unit.

  • The first letter (A or E) defines the type of metering provided by the control unit.

  • If present, a second letter indicates:

    • P: a MicroLogic Active control unit with Zigbee wireless communication.

    • i: a MicroLogic Active control unit without wireless communication.

USB-C Port

The USB-C port is protected by a cover which can be sealed to prevent access by unauthorized personnel. The cover is opened by breaking the seal with a flat screwdriver.

Open the cover of the USB-C port to connect the following devices:

WARNING
hazard of electric shock
Do not use MasterPacT MTZ circuit breakers with MicroLogic Active control units:
  • On power systems with IT grounding system with voltage above 600 Vac.
  • On power systems with other grounding system with voltage above 690 Vac.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: The MicroLogic Active control unit does not support USB keys. Even if a USB key is connected using an adapter, data is not transferred.

Internal Battery

The internal battery powers the trip cause LEDs and the main diagnostic functions in the absence of any other power supply.

For information about testing the internal battery, see Trip Information/Test/Reset Button.

Sensor Plug

The protection ranges depend on the rated current In, defined by the sensor plug present below the MicroLogic Active control unit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.