DOCA0265EN-07

ERMS Function

Engaging the ERMS Function

Step

Action

Screen

1

Use a flat screwdriver to lift the cover of the ERMS button.

2

Press the ERMS button to engage the ERMS function.

3

The ERMS engage request menu opens.

4

Press the ERMS button again, within 10 seconds, to confirm ERMS engagement.

The ERMS loading window is displayed.

5

The ERMS mode activated message is displayed.

6

While the ERMS function is engaged:

  • The ERMS LED is lit in blue.

  • The LSIG home screen is blue.

  • The Quick View screens are blue.

  • All other screens are not blue.

7

Close and seal the cover of the ERMS button.

Disengaging the ERMS Function

Step

Action

Screen

1

Use a flat screwdriver to break the seal and lift the cover of the ERMS button.

2

Press the ERMS button to disengage the ERMS function.

3

The ERMS disengage confirmation menu opens.

4

Press the ERMS button again, within 10 seconds, to confirm ERMS disengagement.

5

Close the cover of the ERMS button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.