DOCA0265EN-07

Trip Information/Test/Reset Button

The button performs the following functions:

  • Trip information

  • Test internal battery and check trip cause LED functionality

  • Reset latched events

Trip Information

After a trip event, press and hold the button for less than 3 seconds for information about the cause of the trip.

When a trip event happens, the related trip cause LED turns off after 2 hours. To re-light the trip cause LED, press the button for less than 3 seconds.

Test

At any time, press and hold the button for less than 3 seconds to test the internal battery and check trip cause LED functionality.

The trip cause LEDs switch off for one second, and then do one of the following:

  • Switch on: the battery is OK.

  • Blink sequentially: the battery is near the end of its life. Replace the battery.

  • Do not light: verify that the plastic battery strip has been correctly removed. If the battery strip has been correctly removed but the LEDs still do not light, then replace the battery

NOTE: This test must be carried out immediately after replacement of the internal battery to check the correct functioning of the new battery. It can then be carried out at any time in the life of the internal battery.

Reset

Press and hold the button for more than 3 seconds to reset latched events, for example trip events.

The trip cause LEDs switch off and the Status bar reverts to green.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.