DOCA0265EN-03

Access Management

General Description

Data on MicroLogic Active control units can be accessed:

The following table describes the functions which can be performed:

Function

Description

Monitoring

Read settings, measurements, and data

Settings

Change MicroLogic Active control unit settings

Reset counters

  • Reset minimum and maximum values

  • Reset operation counters

Test

Send test commands

Firmware update

Update firmware to the latest version

Local Access Management

Local access to data on MicroLogic Active control units is available on the MicroLogic Active control unit HMI.

Local access is protected by a pin code. This pin code has no expiry date.

When you access a protected parameter for the first time, you are prompted to create a SecurityAdmin account and set a pin code. You are then prompted to enter the pin code each time you access a protected parameter. If you enter the wrong pin code 5 times, the account is locked for 4 minutes.

You can postpone account creation by selecting Do it later. In this case, you are prompted to create an account each time you access a protected parameter.

By default, the pin code is associated with the SecurityAdmin account. You can change this account name with EcoStruxure Power Commission software.

The following actions are protected by pin code:

  • HMI pin code modification

  • Protection settings

  • Ground-fault protection test for MicroLogic Active 6.0 control unit

  • Date and time modification

Pin Code Change

The pin code can be changed on the MicroLogic Active control unit HMI.

The pin code must consist of 6 digits, from 0 to 9.

Pin Code Reset

The pin code can be reset by pressing Reset all users when connecting to EcoStruxure Power Commission software or EcoStruxure Power Device app.

After pressing Reset all users, a confirmation pop-up message appears on the screen. Click to confirm and complete the procedure.

Remote Access Management

Remote access to data on MicroLogic Active control units is done with:

  • EcoStruxure Power Device app

  • EcoStruxure Power Commission software

Remote access is protected by a password. This password has no expiry date.

When you connect to EcoStruxure Power Commission software or EcoStruxure Power Device app, you are prompted to create a user name. You can postpone user name creation by selecting Skip.

The default account is SecurityAdmin, and the default password is schneider123. If you decide to create a new user name, you are prompted to create a pin code and password. The user name must not contain special characters.

Password Change

A password can be changed with EcoStruxure Power Commission software.

Entering the current password is required to change the password.

A password is composed of 8 to 32 ASCII characters, with the following constraints:

  • Only ASCII [32–126] allowed

  • At least one uppercase character

  • At least one lowercase character

  • Must not contain the username

  • Must be different to the previous password

Password Reset

The user password of the MicroLogic Active control unit can be reset by pressing Reset Password when connecting to EcoStruxure Power Commission software or EcoStruxure Power Device app.

After pressing Reset Password, a confirmation pop-up message appears on the screen. Click to confirm and complete the procedure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?