DOCA0265EN-07

Monitoring the Internal Functioning of the MicroLogic Active Control Unit

Presentation

The MicroLogic Active control unit carries out a series of self tests to monitor:

  • Correct internal functioning

  • The presence and state of the internal battery

  • The presence of the 24 Vdc power supply

  • The presence of the internal current power supply sensors

  • The temperature inside the control unit

  • Wireless communication

  • The ULP modules:

    • EIFE Ethernet interface

    • IFE Ethernet interface

    • IFM Ethernet interface

Operating Principle

The Ready LED, Status bar, and trip cause LEDs provide visual information about the health state of the MicroLogic Active control unit. The detection of an invalid result in the self tests generates an event (logged in the Diagnostic history) which can be classified as high, medium, or low severity:

  • Low severity event indicates the detection of an invalid result which has no operational impact. The standard (LSIG) protection functions are unaffected.

  • Medium severity event indicates the detection of an invalid result which has a minor operational impact. The standard (LSIG) protection functions are unaffected. A check must be performed at next maintenance.

    • The Ready LED is flashing

    • The Status bar is lit in orange if the event requires non-urgent maintenance

    • All trip cause LEDs are off

    • An orange pop-up screen is displayed

  • High severity event indicates the detection of an invalid result which can have a major operational impact. The standard (LSIG) protection functions can be affected. The control unit must be replaced without delay.

    • The Ready LED is off

    • The Status bar is lit in red if the event requires immediate maintenance

    • All trip cause LEDs are lit

    • A red pop-up screen is displayed

When monitoring of the internal functioning of MicroLogic Active control unit detects an invalid result with medium or high severity, an event is generated with an orange or red pop-up screen and corresponding event message.

Setting Change Not Applied

The MicroLogic Active control unit monitors progress when protection settings are changed, and generates the Last protection settings have not been applied event if the new protection settings are unable to be applied.

Data Availability

Monitoring data is available as follows:

  • On the MicroLogic Active display screen.

  • With EcoStruxure Power Commission software for all severities

  • With EcoStruxure Power Device app through USB OTG connection for medium and high severities.

  • With the Zigbee wireless communication network for MicroLogic Active AP/EP control units.

  • On a server or remote controller using the wired communication network

Restarting MicroLogic Active Control Unit

If the display screen of the MicroLogic Active control unit no longer displays menus for protection, alarms, or measures screens, it is recommended to restart the MicroLogic Active control unit.

Predefined Events

The function generates the following events:

Code

Event

History

Severity

0x4005 (16389)

Control unit over temperature trip

Trip

High

0x1404 (5124)

Control unit over temperature

Diagnostic

High

0x142F (5167)

Last protection settings have not been applied.

Diagnostic

Medium

0x140F (5135)

Protection settings not accessible 1

Diagnostic

Medium

0x1474 (5236)

Protection settings not accessible 2

Diagnostic

Medium

0x1473 (5235)

Internal access loss. Reboot control unit

Diagnostic

Medium

0x1436 (5174)

Control unit memory degradation

Diagnostic

Low

0x0D00 (3328)

Critical hardware modules discrepancy

Diagnostic

Medium

0x0D01 (3329)

Critical firmware modules discrepancy

Diagnostic

Medium

0x0D02 (3330)

Non-critical hardware modules discrepancy

Diagnostic

Medium

0x0D03 (3331)

Non-critical firmware modules discrepancy

Diagnostic

Medium

0x0D09 (3337)

Firmware discrepancy within control unit.

Diagnostic

Medium

0x1433 (5171)

Replace internal battery

Diagnostic

Low

0x1437 (5175)

Internal battery not detected

Diagnostic

Low

0x150F (5391)

Iron CT loss. Replace circuit breaker.

Diagnostic

High

0x0D0A (3338)

Invalid CU factory config. 1

Diagnostic

Medium

0x1122 (4386)

Communication lost with EIFE or IFE module

Diagnostic

Medium

0x1123 (4387)

Communication lost with IFM module

Diagnostic

Medium

Recommended Actions

Code

Event

Recommended actions

0x4005 (16389)

Control unit over temperature trip

Decrease ambient temperature near the circuit breaker. If the problem persists, replace the MicroLogic Active control unit.

0x1404 (5124)

Control unit over temperature

Decrease ambient temperature near the circuit breaker. If the problem persists, replace the MicroLogic Active control unit.

0x142F (5167)

Last protection settings have not been applied.

Apply again the protection settings.

0x140F (5135)

Protection settings not accessible 1

Plan to replace the MicroLogic Active control unit.

0x1474 (5236)

Protection settings not accessible 2

Reboot control unit by simultaneously pressing the 5 buttons , OK, Back, Up, Down. If the event recurs, plan to replace the MicroLogic Active control unit.

0x1473 (5235)

Internal access loss. Reboot control unit

Internal access loss. Reboot control unit by simultaneously pressing the 5 buttons , OK, Back, Up, Down.

0x1436 (5174)

Control unit memory degradation

Plan to replace the MicroLogic Active control unit.

0x0D00 (3328)

Critical hardware modules discrepancy

Check which module is in critical hardware discrepancy with the EcoStruxure Power Commission software Firmware menu. Replace the module.

0x0D01 (3329)

Critical firmware modules discrepancy

Check which module is in critical firmware discrepancy with the EcoStruxure Power Commission software. Update the module.

0x0D02 (3330)

Non-critical hardware modules discrepancy

Check which module is in non-critical hardware discrepancy with the EcoStruxure Power Commission software Firmware menu. Plan to replace the module.

0x0D03 (3331)

Non-critical firmware modules discrepancy

Check which module is in non-critical firmware discrepancy with the EcoStruxure Power Commission software. Plan to update the module.

0x0D09 (3337)

Firmware discrepancy within control unit.

Check the firmware version of the MicroLogic Active control unit with EcoStruxure Power Commission software. If not latest, update the firmware of the MicroLogic Active control unit.

0x1433 (5171)

Replace internal battery

Replace internal battery. Connect a Mobile Power Pack to the USB-C port during internal battery replacement, to avoid losing date and time information.

0x1437 (5175)

Internal battery not detected

Install internal battery.

0x150F (5391)

Iron CT loss. Replace circuit breaker.

Replace the circuit breaker.

0x0D0A (3338)

Invalid CU factory config. 1

Plan to replace the MicroLogic Active control unit.

0x1122 (4386)

Communication lost with EIFE or IFE module

Check the power supply of the EIFE or IFE module. Check the ULP cable connection.

0x1123 (4387)

Communication lost with IFM module

Check the power supply of the IFM module. Check the ULP cable connection.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Internal Battery Replacement

The internal battery of the MicroLogic Active control unit can be replaced on site when discharged. The replacement can be made with the circuit breaker in the open or closed position, and the control unit supplied with power. A test of the internal battery must be carried out immediately after the replacement of the internal battery to check the correct functioning of the new battery.

For information about internal battery replacement and installation, consult the instruction sheet on the Schneider Electric website: PKR4244002MicroLogic Active - Spare Battery - Instruction Sheet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.