DOCA0265EN-07

Perform a Primary Injection Test

Description

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Perform a primary injection test on each pole of the circuit breaker to check that the MicroLogic Active control unit is able to provide standard protection functions.
Failure to follow these instructions will result in death or serious injury.

A primary injection test on each pole of the circuit breaker is mandatory to check that trip system connections have been correctly made and that the MicroLogic Active control unit is able to provide standard protection functions, for example tripping the circuit breaker in case of an electrical network incident. The test is performed by injecting a controlled current from an external power source, into the primary circuit of the circuit breaker.

Preparing the Primary Injection Test

A wiring diagram of the primary injection test kit for MasterPacT MTZ1 and MasterPacT MTZ2 circuit breakers is illustrated below.

Use 2.5 mm2 cables between R1 and CTR1.

B1

MCB circuit breaker 10 A

T1

Transformer 250 VA

B2

MCB circuit breaker 16 A

CTR1

Control relay

P.B.

Pushbutton

R1

Resistance 300 W - 2.2 Ohms

J1

Jaws for connection to the upstream and equivalent downstream of one pole

Bill of Materials

Schneider Electric recommends the following components for the primary injection test kit for MasterPacT MTZ1 and MasterPacT MTZ2 circuit breakers.

Schematic reference

Item

Supplier

Reference

Quantity

B1

Circuit breaker DT40 – 10 A + Vigi 30 mA

Schneider Electric

A9D55610

1

T1

Transformer 250VA 220 Vac – 24 Vac

BLOCK

FST 250/24

1

B2

Circuit breaker DT40 – 16 A + Vigi 30 mA

Schneider Electric

A9N21025+

A9N21454

1

CTR1

Auxiliary Zelio relay

Schneider Electric

RSB2A080B7

1

P.B

Pushbutton with normally open contact

Schneider Electric

XB4BL41

1

R1

Resistor 2.2 ohms – 300 W

WIDAP

160169

1

Conrad

1525215

1

J1

Jaws

GRELUMA

ZL373LUM

2

Terminal block for multimeter connection

Schneider Electric

47075

2

NOTE: For the MasterPacT MTZ3 primary injection test kit, contact Schneider Electric Customer Care.

Performing the Primary Injection Test

Perform this test on each pole of the circuit breaker.

Step

Action

1

Disconnect the circuit breaker from the switchboard network before starting.

2

Charge the mechanism by pulling the spring charging handle down seven times.

3

Close the circuit breaker by pressing the closing pushbutton on the front of the circuit breaker.

4

Connect the primary circuit of the circuit breaker to the kit using the jaws (J1), as shown in the wiring diagram above.

  • Use 10 A 24 Vac for MasterPacT MTZ1 and MasterPacT MTZ2 circuit breakers.

  • Use 30 A 24 Vac for MasterPacT MTZ3 circuit breakers.

Connect the external power source to the upstream and downstream of one pole.

5

  • Connect the positive probe of the multimeter to M1 on the UC1 terminal block.

  • Connect the negative probe of the multimeter to M3 on the UC2 terminal block.

6

Press the pushbutton to inject current into the circuit breaker.

7

Wait until the voltage reading is greater than 1 Vdc.

8

The test passes if the measured voltage is greater than 1 Vdc.

Example of a Primary Injection Test Kit

A

Circuit breaker block

B

Jaw connected to upstream pole

C

Primary injection test kit

D

Jaw connected to downstream pole

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.