DOCA0265EN-07

MicroLogic Active Measurement Characteristics

Presentation

The following tables indicate the measurements available in MicroLogic Active control units and specify the following information for each measurement:

  • Unit

  • Measurement range

Current

Measurement

Unit

Range

  • Real-time phase current values I1, I2, I3

  • Maximum phase current values I1 Max, I2 Max, I3 Max

  • Minimum phase current values I1 Min, I2 Min, I3 Min

A

0(1)–20 In

  • Real-time neutral current value IN(2)

  • Maximum neutral current value IN Max(2)

  • Minimum neutral current value IN Min(2)

A

0(1)–20 In

  • Real-time average current value I Avg(3)

  • Minimum average current value Iavg Min

A

0(1)–20 In

  • Real-time ground-fault current value Ig

  • Maximum value of the ground-fault current Ig Max

  • Minimum value of the ground-fault current Ig Min

A

0–20 In

(1) If the current falls below the lowest measurable current, the measurement reverts to 0 A.

  • For MasterPacT MTZ1/MTZ2 circuit breaker, the lowest measurable current is:

    • 15 A when In ≥ 400 A.

    • 5 A when In < 400 A.

  • For MasterPacT MTZ3 circuit breaker, the lowest measurable current is 30 A.

(2) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENCT wired and configured.

(3) Applies to MicroLogic Active E/EP/Ei control unit only.

Current Unbalance (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Real-time maximum of 3 phase current unbalances

  • Maximum of maximum of 3 phase current unbalances

0–100%

Current Demand (MicroLogic Active E/EP/Ei)

Measurement

Unit

Range

  • Phase (I1, I2, I3, Iavg) current demand values

  • Phase (I1, I2, I3, Iavg) peak current demand values

A

0–20 In

  • Neutral (IN) current demand value(1)

  • Neutral (IN) peak current demand value(1)

A

0–20 In

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENCT wired and configured.

Operating Indicators

Measurement

Range

Phase rotation

123 or 132

Type of load

Leading or Lagging (IEEE)

Capacitive or Inductive (IEC)

Voltage (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Real-time phase-to-phase voltage values V12, V23, V31

  • Maximum values of phase-to-phase voltages V12 MAX, V23 MAX, V31 MAX

  • Minimum values of phase-to-phase voltages V12 MIN, V23 MIN, V31 MIN

0(1)–1,150 V

  • Real-time phase-to-neutral voltages V1N, V2N, V3N(2)

  • Maximum values of phase-to-neutral voltages V1N MAX, V2N MAX, V3N MAX(2)

  • Minimum values of phase-to-neutral voltages V1N MIN, V2N MIN, V3N MIN(2)

0(1)–660 V

  • Real-time average phase-to-phase voltage Vavg LL

0(1)–1,150 V

  • Real-time average phase-to-neutral voltage Vavg LN(2)

0(1)–600 V

(1) If the voltage falls below the lowest measurable voltage (10 V), the measurement reverts to 0 V.

(2) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Voltage Unbalance (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Real-time maximum of 3 phase-to-phase voltage unbalances VLL Unb

0–100%

  • Real-time maximum of 3 phase-to-neutral voltage unbalances VLN Unb(1)

0–100%

  • Maximum of maximum of 3 phase-to-phase voltage unbalances VLL Unb Max

0–100%

  • Maximum of maximum of 3 phase-to-neutral voltage unbalances VLN Unb Max(1)

0–100%

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Real-time active power for each phase P1, P2, P3(1)

  • Maximum values of active power for each phase P1 MAX, P2 MAX, P3 MAX(1)

-16,000– +16,000 kW

  • Real-time total active power Ptot

  • Maximum value of total active power Ptot MAX

-16,000– +16,000 kW

  • Real-time reactive power for each phase Q1, Q2, Q3(1)

  • Maximum values of reactive power for each phase Q1 MAX, Q2 MAX, Q3 MAX(1)

-16,000– +16,000 kvar

  • Real-time total reactive power Qtot

  • Maximum value of total reactive power Qtot MAX

-16,000– +16,000 kvar

  • Real-time apparent power for each phase S1, S2, S3(1)

  • Maximum values of apparent powers for each phase S1 MAX, S2 MAX, S3 MAX(1)

-16,000– +16,000 kVA

  • Real-time total apparent power Stot

  • Maximum value of total apparent power Stot MAX

-16,000– +16,000 kVA

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power Demand (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Total active power demand value

  • Total peak active power demand value

-16,000– +16,000 kW

  • Total reactive power demand value

  • Total peak reactive power demand value

-16,000– +16,000 kvar

  • Total apparent power demand value

  • Total peak apparent power demand value

-16,000– +16,000 kVA

Power Factor PF and cos φ (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Real-time total power factor PF

  • Maximum value of the total power factor PF Max

  • Minimum value of the total power factor PF Min

-1.00–+1.00

  • Real-time total cos φ

  • Maximum cos φ Max

  • Minimum cos φ Min

-1.00–+1.00

Real-time power factors for each phase PF1, PF2, PF3(1)

-1.00–+1.00

  • Maximum power factor for each phase PF1 Max, PF2 Max, PF3 Max(1)

  • Minimum power factor for each phase PF1 Min, PF2 Min, PF3 Min(1)

-1.00–+1.00

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Frequency (MicroLogic Active E/EP/Ei)

Measurement

Range

  • Frequency

  • Maximum frequency

  • Minimum frequency

40–70 Hz

Resettable Energy Meters (MicroLogic Active E/EP/Ei)

Measurement

Range

Total active energy value Ep

-10,000,000 to +10,000,000 kWh

Total active energy values Ep delivered and Ep received

-10,000,000 to +10,000,000 kWh

Total reactive energy value Eq

-10,000,000 to +10,000,000 kvarh

Total reactive energy values Eq delivered and Eq received

-10,000,000 to +10,000,000 kvarh

Apparent energy Es

-10,000,000 to +10,000,000 kVAh

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.