DOCA0265EN-07

Test the Microswitch

If the microswitch is present, it is recommended to test the microswitch.

Test the Microswitch by Using ULP Wired Communication

Test the microswitch by verifying that the status of the circuit breaker can be read from the Modbus tables.

For more information, refer to DOCA0384•• MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

Test the Microswitch by Using Zigbee Wireless Communication

For MicroLogic Active AP/EP control units, test the microswitch by verifying that the status of the circuit breaker is available on Panel Server webpages.

Step

Action

1

Select the Monitoring & Control menu on Panel Server webpages.

2

Select the MasterPacT MTZ circuit breaker with MicroLogic Active AP/EP control unit to test, from the list of connected devices.

3

Check the circuit breaker status.

4

If the circuit breaker status (open or closed), displayed on Panel Server webpages does not match the actual status of the circuit breaker, the microswitches are not correctly connected to the MicroLogic Active AP/EP control unit. Repeat the procedure to replace the control unit.

If the problem persists, contact your Schneider Electric Services representative.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.