DOCA0265EN-07

Event History

Overview

All events are logged in one of the histories of the MicroLogic Active control unit:

  • Trip

  • Protection

  • Diagnostic

  • Operation

Events of all severity are logged, including low-severity events.

Event histories are encrypted by using the AES-256 encryption algorithm.

Events logged in histories are displayed as follows:

  • On the MicroLogic Active display screen

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

The trip history can be downloaded by using the wired communication network.

The following information is logged in a history for each event:

  • Event ID: event code

  • Time stamp: date and time of occurrence and completion

The trip history on the MicroLogic Active display screen additionally includes context data (protection settings, interrupted currents).

NOTE: The MicroLogic Active HMI displays the date and time of occurrence of events. The date and time of completion of events can be consulted by extracting MicroLogic Active control unit histories:
  • Through EcoStruxure Power Commission software.

  • Through EcoStruxure Power Device app.

Maximum Number of Events in Each History

Each history has a predefined maximum size. When a history is full, each new event overwrites the oldest event in the relevant history.

Event history

Maximum number of events stored in history

Trip

30

Protection

50

Diagnostic

200

Operation

160

Displaying Event History on MicroLogic Active Display Screen

For more information about how events are displayed on MicroLogic Active display screen, refer to Alarms/History menu.

Displaying Event History on EcoStruxure Power Commission Software

All events logged in histories can be consulted using EcoStruxure Power Commission software. The events can be exported as an Excel file.

Events in histories are displayed in chronological order, starting with the most recent event.

Displaying Event History on EcoStruxure Power Device App

All events logged in histories are displayed on the EcoStruxure Power Device app.

Events in histories are displayed in chronological order, starting with the most recent event.

Events can be sorted by date and time, or by sequence number, and filtered by using the following criteria:

  • Type

  • Severity

  • History

Clicking on a specific event in the list displays a list of all occurrences of the same event, in chronological order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.