DOCA0265EN-07

Event Notifications

Presentation

High severity events (including trips) and medium severity events are notified by a pop-up screen on the MicroLogic Active control unit.

Trip events are notified by SDE1 standard fault-trip indication contact and SDE2 optional fault-trip indication contact.

In addition, events can be configured to be notified in the following ways:

  • By optional BCIM module.

  • By email from IFE or EIFE Ethernet interface.

  • By email from Panel Server.

Pop-up Screen

All high and medium severity events generate a pop-up screen on the MicroLogic Active display screen:

  • A red pop-up screen indicates a trip or high severity event, needing immediate attention.

  • An orange pop-up screen indicates a medium severity event, recommending action.

BCIM Module Notification

When configured in Alarm mode, the optional BCIM module can be used to signal the status of alarms.

The BCIM module is equipped with two outputs to activate external pilot lights when the alarms are active.

To configure the BCIM module in Alarm mode, set the BCIM parameters on the MicroLogic Active display screen, at Configuration > BCIM as follows:

  • BCIM = Yes

  • IO Settings > IO Mode = Alarm

  • Select one event to be signaled on each IO Channel, from the following:

BCIM channel

IO channel alarm

Event

Code

IO channel 1

Long Time (Start)

Ir start (I > 105% Ir)

0x6200 (25088)

Short Time (Start)

Isd start

0x6201 (25089)

Ground Fault (Start)

Ig start

0x6203 (25091)

IO channel 2

Long Time (Trip)

Long Time (Ir) trip

0x4000 (16384)

Short Time (Trip)

Short Time (Isd) trip

0x4001 (16385)

Instantaneous (Trip)

Instantaneous (Ii) trip

0x4002 (16386)

Ground Fault (Trip)

Ground Fault (Ig) trip

0x4003 (16387)

Email Notification from IFE/EIFE Interfaces

IFE or EIFE webpages allow events to be selected for notification by email. The notification by email is not configured by default.

For more information, refer to the relevant document:

  • Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

  • Enerlin'X IFE – Ethernet Interface for One IEC Circuit Breaker – User Guide

  • Enerlin'X IFE - Ethernet Switchboard Server - User Guide

Email Notification from Panel Server

For MicroLogic Active AP/EP control unit, the last event can be configured to be notified by email from Panel Server. The notification by email is not configured by default. For more information, refer to DOCA0172•• EcoStruxure Panel Server - User Guide.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.