DOCA0265EN-07

Presentation

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not install a MicroLogic Active control unit with version number less than 004.000.000 in a MasterPacT MTZ circuit breaker with performance level L1 or H3.
Failure to follow these instructions will result in death or serious injury.

The replacement procedure described in this guide specifically applies to:

  • The replacement of a MicroLogic Active control unit embedded in a MasterPacT MTZ circuit breaker, by another MicroLogic Active control unit.

  • The removal and reinstallation of a MicroLogic Active control unit embedded in a MasterPacT MTZ circuit breaker, for example during the replacement of an accessory.

NOTE: Replacement of a MicroLogic Active control unit in MasterPacT NT/NW circuit breakers must be carried out by accredited Schneider Electric Services representatives or accredited Schneider Electric certified partners.

In all cases, the replacement procedure must be followed by the compulsory tests to perform after reinstallation of the MicroLogic Active control unit.

Replacement Process

Test Required After MicroLogic Active Control Unit Replacement

Test requirement

Test description

Mandatory

Perform a primary injection test on each pole of the circuit breaker.

Mandatory

Perform a trip test.

Recommended

Perform a secondary injection test.

Recommended

Test the internal battery.

Recommended

If the microswitch is present, test the microswitch.

Recommended

If the BCIM module is present, test circuit breaker communication.

Recommended

If the BCIM module is present and remote control of the circuit breaker is enabled, test the remote control operation.

MicroLogic Active Replacement Video

To access a demonstration video about replacement of a MicroLogic Active control unit, click here, scan the QR code, or copy and paste the link to your Web browser:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.