DOCA0265EN-07

MicroLogic Active Measurement Availability and Display

Presentation

The available measurements depend on the type of MicroLogic Active control unit:

  • MicroLogic Active A/AP control unit measures currents only.

  • MicroLogic Active E/EP/Ei control unit measures currents and voltages.

The measurements can be displayed :

  • On the MicroLogic Active display screen

  • On the FDM121 display

  • With Panel Server Zigbee connectivity: on Panel Server webpages and on remote controllers connected to Panel Server, through Zigbee wireless communication (MicroLogic Active AP/EP control unit only)

  • On a server or remote controller using the wired communication network

  • On IFE/EIFE webpages

The following tables indicate which measurements are available on each type of display option.

Current

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time phase current values I1, I2, I3

Maximum phase current values I1 Max, I2 Max, I3 Max

Minimum phase current values I1 Min, I2 Min, I3 Min

Real-time neutral current value IN(1)

Maximum neutral current value IN Max(1)

Minimum neutral current value IN Min(1)

Real-time average current value I Avg(2)

Minimum average current value Iavg Min

Real-time ground-fault current value Ig

Maximum value of the ground-fault current Ig Max

Minimum value of the ground-fault current Ig Min

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENCT wired and configured.

(2) Applies to MicroLogic Active E/EP/Ei control unit only.

Current Unbalance (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time maximum of 3 phase current unbalances I Unb

Maximum of maximum of 3 phase current unbalances I Unb Max

Current Demand (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Phase (I1, I2, I3) current demand values

Phase (Iavg) current demand values

Phase (I1, I2, I3) peak current demand values

Phase (Iavg) peak current demand values

Neutral (IN) current demand value(1)

Neutral (IN) peak current demand value(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Operating Indicators (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Phase rotation

Type of load

Voltage (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time phase-to-phase voltage values V12, V23, V31

Maximum values of phase-to-phase voltages V12 MAX, V23 MAX, V31 MAX

Minimum values of phase-to-phase voltages V12 MIN, V23 MIN, V31 MIN

Real-time phase-to-neutral voltages V1N, V2N, V3N(1)

Maximum values of phase-to-neutral voltages V1N MAX, V2N MAX, V3N MAX(1)

Minimum values of phase-to-neutral voltages V1N MIN, V2N MIN, V3N MIN(1)

Real-time average phase-to-phase voltage Vavg LL

Real-time average phase-to-neutral voltage Vavg LN(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Voltage Unbalance (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time maximum of 3 phase-to-phase voltage unbalances VLL Unb

Real-time maximum of 3 phase-to-neutral voltage unbalances VLN Unb(1)

Maximum of maximum of 3 phase-to-phase voltage unbalances VLL Unb Max

Maximum of maximum of 3 phase-to-neutral voltage unbalances VLN Unb Max(1)

Real-time phase-to-phase voltage unbalances V12unbal, V23unbal, V31unbal

Real-time phase-to-neutral voltage unbalances V1Nunbal, V2Nunbal, V3Nunbal(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time active power for each phase P1, P2, P3(1)

Maximum values of active power for each phase P1 MAX, P2 MAX, P3 MAX(1)

Real-time total active power Ptot

Maximum value of total active power Ptot MAX

Real-time reactive power for each phase Q1, Q2, Q3(1)

Maximum values of reactive powers for each phase Q1 MAX, Q2 MAX, Q3 MAX(1)

Real-time total reactive power Qtot

Maximum value of total reactive power Qtot MAX

Real-time apparent power for each phase S1, S2, S3(1)

Maximum values of apparent powers for each phase S1 MAX, S2 MAX, S3 MAX(1)

Real-time total apparent power Stot

Maximum value of total apparent power Stot MAX

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Power Demand (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Total active power demand value

Total peak active power demand value

Total reactive power demand value

Total peak reactive power demand value

Total apparent power demand value

Total peak apparent power demand value

Power Factor PF and cos φ (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Real-time total power factor PF

  • Maximum value of the total power factor PF Max

  • Minimum value of the total power factor PF Min

Real-time total cos φ

  • Maximum cos φ Max

  • Minimum cos φ Min

Real-time power factors for each phase PF1, PF2, PF3(1)

  • Maximum power factor for each phase PF1 Max, PF2 Max, PF3 Max(1)

  • Minimum power factor for each phase PF1 Min, PF2 Min, PF3 Min(1)

(1) Applies to 4-pole circuit breakers or 3-pole circuit breakers with ENVT wired and configured.

Frequency (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Frequency

Maximum frequency

Minimum frequency

Resettable Energy Meters (MicroLogic Active E/EP/Ei)

Measurement

MicroLogic Active HMI

FDM121

Panel Server Zigbee connectivity

Wired communication network

IFE/EIFE webpages

Total active energy value Ep

Total active energy values: Ep delivered, and Ep received

Active energy values for each phase: Ep1 delivered, Ep2 delivered, Ep3 delivered, Ep1 received, Ep2 received, Ep3 received

Total reactive energy value Eq

Total reactive energy values: Eq delivered, and Eq received

Reactive energy values for each phase: Eq1 delivered, Eq2 delivered, Eq3 delivered, Eq1 received, Eq2 received, Eq3 received

Total apparent energy value Es

Apparent energy value for each phase Es1, Es2, Es3

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.