DOCA0265EN-07

Alarms/History Menu

Description

The Alarms/History menu contains the following menus:

Level 1

Level 2

Level 3

Function description

Tree navigation menu

Alarms/History

Active Alarms

Displays events of medium and high severity of entry/exit type, after the occurrence of the alarm and before the completion.

Trips are not displayed.

Trips history

Displays the history of trips, with the date and time that the trip occurred.

Alarms history

Displays the history of events of medium and high severity, with the date and time that the alarm occurred.

Trips are not displayed in this history.

NOTE: Trip history and alarm history events are listed in chronological order, with the most recent event first. Events are only listed in chronological order if the internal battery is working.

Active Alarms Screens

An active alarms screen contains the following information:

  • Screen title: Active Alarms

  • A list of active alarms with the date and time of occurrence.

Use the up/down buttons and OK button to navigate between active alarm screens.

Trips History Screens

A trips history screen contains the following information:

  • Screen title: Trips history

  • A list of trip events with the date and time of occurrence.

Trips history events are listed in chronological order, with the most recent event first.

NOTE: Events are only listed in chronological order if the internal battery is working.

Use the up/down buttons and OK button to navigate to a trip event description screen.

Alarms History Screens

An alarms history screen contains the following information:

  • Screen title: Alarms history

  • A list of alarm events with the date and time of occurrence. A symbol next to an alarm event indicates the severity of the alarm.

    • A red triangle indicates a high severity alarm.

    • An orange diamond indicates a medium severity alarm.

Alarms history events are listed in chronological order, with the most recent event first.

NOTE: Events are only listed in chronological order if the internal battery is working.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.