DOCA0265EN-07

Health State

Presentation

The health state of the circuit breaker is determined from the following functions:

The health state of the circuit breaker is displayed on the Health screen and the Status bar.

For more information, refer to the list of events.

Health Screen

The Health screen displays one of the following screens:

Good health state (green)

Medium-severity detected alarm that requires non-urgent action (orange)

High-severity detected alarm that requires immediate corrective action (red)

Status Bar

The Status bar:

  • Is lit in green under normal operating conditions.

  • Is lit in orange in the case of a medium severity alarm which requires non-urgent maintenance action.

  • Is lit in red in the case of a high severity alarm which requires immediate maintenance action.

  • Blinks red in the case of a trip event.

Data Availability

The health state is available:

  • On the MicroLogic Active HMI Health screen during Quick View scrolling.

  • With the Zigbee wireless communication network for MicroLogic Active AP/EP control units.

  • On a server or remote controller using the wired communication network

When a high or medium severity event is detected a pop-up screen is displayed. If the pop-up is acknowledged by pressing OK, the display returns to Quick View scrolling, and the Health screen is displayed again.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.