DOCA0265EN-07

Firmware Update

Introduction

The primary reason for updating the firmware of a MicroLogic Active control unit is to obtain the latest MicroLogic Active features. If the latest MicroLogic Active features are not required, it is not mandatory to update the firmware of the MicroLogic Active control unit and the devices of the IMU.

The standard protection functions of the MicroLogic Active control unit remain active during a firmware update.

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

For more information about firmware updates refer to the following documents:

  • DOCA0155•• MicroLogic Trip Units and Control Units - Firmware History

  • DOCA0267•• MasterPacT MTZ - MicroLogic Active Control Unit - Firmware Release Notes

  • DOCA0387•• Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - User Guide

  • DOCA0395•• Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - Firmware Release Notes

After updating the firmware version of the MicroLogic Active control unit, use the Firmware Update table in EcoStruxure Power Commission software to check firmware compatibility with the BCIM module.

NOTE: Only the compatibility of MicroLogic Active control unit and the BCIM module is checked. The firmware of the other modules of the ULP system must be checked separately.

Checking the Firmware Version

Check the firmware version:

  • On the MicroLogic Active display screen from the tree navigation menu, at Maintenance > Assistance > Firmware version

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

Updating Firmware With EcoStruxure Power Commission Software

NOTICE
INTERRUPTION OF POWER SUPPLY
The MicroLogic Active control unit must be continuously powered during the firmware update.
Failure to follow these instructions will result in deterioration of the control unit.

The prerequisites for updating the firmware with EcoStruxure Power Commission software are the following:

  • The latest version of EcoStruxure Power Commission software must be downloaded and installed on the PC.

  • The PC must be connected to a power supply. Standby mode must be deactivated to avoid the possibility of interruption during the update.

  • The PC must be connected to the USB-C port on the MicroLogic Active control unit.

  • The MicroLogic Active control unit must be powered by the PC.

The user must be authenticated and have the related permission to launch the firmware update.

For more information, refer to EcoStruxure Power Commission Online Help.

Click here to download the latest version of EcoStruxure Power Commission software.

Predefined Events

The following events can be generated when a firmware update is performed:

Code

Event

History

Severity

0x0D09 (3337)

Firmware discrepancy within control unit.

Diagnostic

Medium

0x112B (4395)

Control unit firmware update mode

Operation

Low

0x112C (4396)

Control unit firmware update unsuccessful

Operation

Low

Recommended Actions

Code

Event

Recommended actions

0x0D09 (3337)

Firmware discrepancy within control unit.

Check the firmware version of the MicroLogic Active control unit with EcoStruxure Power Commission software. If not latest, update the firmware of the MicroLogic Active control unit.

0x112B (4395)

Control unit firmware update mode

Wait until the update of the MicroLogic control unit firmware is completed.

0x112C (4396)

Control unit firmware update unsuccessful

Restart the update procedure. If the message is displayed again, plan to replace the MicroLogic Active control unit.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.