DOCA0265EN-07

Monitoring the Contact Wear

Presentation

The pole contacts undergo wear due to the number of operating cycles with current and interrupted current during short circuits. It is recommended to check them at periodic intervals to decide whether the contacts must be changed or not. In order to reduce systematic visual inspections of the contacts and the arc chute, the contact wear estimate helps with the planning of visual inspections based on the estimated wear (from 0% - new contact - to 100% - totally worn contact).

Operating Principle

Each time the circuit breaker operates (performs an open and close cycle with or without current), the corresponding mechanical and electrical operation counters are incremented. Based on these counters, the MicroLogic Active control unit calculates the contact wear.

When the MicroLogic Active control unit contact wear algorithm calculates a value which is above one of the predefined thresholds (60%, 95%, and 100%) an event is generated with an orange or red pop-up screen and corresponding event message.

Data Availability

Contact wear monitoring data is available:

  • On the MicroLogic Active display screen, from the tree navigation menu, at Maintenance > Health > Contact wear

  • With the Zigbee wireless communication network for MicroLogic Active AP/EP control units.

  • On a server or remote controller using the wired communication network

Circuit breaker operation counters are available on a server or remote controller using the wired communication network.

Predefined Events

The function generates the following events:

Code

Event

History

Severity

0x1440 (5184)

Contact wear > 60%. Check contacts.

Diagnostic

Medium

0x1441 (5185)

Contact wear > 95%. Plan circuit breaker replacement.

Diagnostic

Medium

0x1442 (5186)

Contact wear > 100%. Replace circuit breaker.

Diagnostic

High

Recommended Actions

Code

Event

Recommended actions

0x1440 (5184)

Contact wear > 60%. Check contacts.

Inspect visually the arc chute and main contacts at the next scheduled maintenance.

0x1441 (5185)

Contact wear > 95%. Plan circuit breaker replacement.

Plan to replace the circuit breaker.

0x1442 (5186)

Contact wear > 100%. Replace circuit breaker.

Replace the circuit breaker.

Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.