DOCA0265EN-07

Monitoring the Tripping Circuit

Presentation

When the MicroLogic Active control unit is energized, it provides constant monitoring of the following:

  • The internal tripping circuit

  • The connection of the internal sensors (internal current transformers, sensor plug, performer plug)

  • The connection of the circuit breaker tripping voltage release (MITOP) to the MicroLogic Active control unit

  • The connection of the ENCT (External Neutral Current Transformer)

NOTE: The mechanism is not monitored. It is recommended to perform preventive maintenance as proposed by Schneider Electric. For more information, refer to DOCA0305•• MasterPacT MTZ IEC Circuit Breakers with MicroLogic Active Control Unit - Maintenance Guide.

Operating Principle: Ready LED

  1. Ready LED

The result of the monitoring is indicated by the Ready LED on the front face of the MicroLogic Active control unit, as follows:

  • The Ready LED is flashing green: the internal tripping circuit of the circuit breaker is functioning correctly.

  • The Ready LED is off, which indicates one of two scenarios:

    • The MicroLogic Active control unit is not energized. In this case, provide power to the control unit with a Mobile Power Pack. If the Ready LED is still off, consult the history of active events on the MicroLogic Active display screen, from the tree navigation menu, at Alarms/History > Active Alarms to diagnose the situation.

    • There is a detected incident in the tripping circuit. Consult the history of active events on the MicroLogic Active display screen, from the tree navigation menu, at Alarms/History > Active Alarms to diagnose the situation.

Circuit Breaker Status

Following the detection of an incident in the tripping circuit the circuit breaker may be tripped or not, depending on the type of incident detected.

Unable to Read Sensor Plug

When the MicroLogic Active control unit is unable to read the rated current In from the sensor plug, the event Unable to read sensor plug is generated and the value of the rated current In is forced:

  • In = 400 A for MasterPacT MTZ1/MTZ2 circuit breaker

  • In = 800 A for MasterPacT MTZ3 circuit breaker

The protection settings based on the value of In are modified accordingly.

Tripping Data and Availability

The following data about the tripping function is logged by the MicroLogic Active control unit:

  • Total number of trips

  • The name and date of the most recent trip

The tripping data is available:

  • With EcoStruxure Power Commission software.

  • With EcoStruxure Power Device app through NFC and USB OTG connection.

  • With the Zigbee wireless communication network for MicroLogic Active AP/EP control units.

  • On a server or remote controller using the wired communication network

    Predefined Events

    The monitoring of the tripping circuit generates the following events:

    Code

    Event

    History

    Severity

    0x4007 (16391)

    Self diagnostic trip. Replace control unit

    Trip

    High with trip

    0x400A (16394)

    ENCT Disconnected trip

    Trip

    High with trip

    0x4033 (16435)

    Current sensor loss. Replace Circuit Breaker

    Trip

    High with trip

    0x1400 (5120)

    Self test 1. Replace control unit

    Diagnostic

    High with trip

    0x1404 (5124)

    Control unit over temperature

    Diagnostic

    High with trip

    0x1405 (5125)

    Self test 3. Replace control unit

    Diagnostic

    High with trip

    0x1406 (5126)

    Self test 4. Replace control unit

    Diagnostic

    High with trip

    0x1416 (5142)

    Mitop disconnected. Call Schneider Electric support

    Diagnostic

    High with trip

    0x1402 (5122)

    Current sensor loss. Replace circuit breaker.

    Diagnostic

    High with trip

    0x1403 (5123)

    ENCT disconnected

    Diagnostic

    High with trip

    0x1430 (5168)

    Protection settings reset to factory values

    Diagnostic

    High

    0x1409 (5129)

    Unable to read sensor plug

    Diagnostic

    High

    0x1518 (5400)

    Self-test 6. Replace control unit.

    Diagnostic

    High

    Recommended Actions

    Code

    Event

    Recommended actions

    0x4007 (16391)

    Self diagnostic trip. Replace control unit

    Replace the MicroLogic Active control unit. Contact Schneider Electric Support.

    0x400A (16394)

    ENCT Disconnected trip

    Check internal/external wiring of External Neutral Current Transformer (ENCT).

    0x4033 (16435)

    Current sensor loss. Replace Circuit Breaker

    Replace the circuit breaker. Contact Schneider Electric Support.

    0x1400 (5120)

    Self test 1. Replace control unit

    Replace the MicroLogic Active control unit. Contact Schneider Electric Support.

    0x1404 (5124)

    Control unit over temperature

    Decrease ambient temperature near the circuit breaker. If the problem persists, replace the MicroLogic Active control unit.

    0x1405 (5125)

    Self test 3. Replace control unit

    Replace the MicroLogic Active control unit. Contact Schneider Electric Support.

    0x1406 (5126)

    Self test 4. Replace control unit

    Replace the MicroLogic Active control unit. Contact Schneider Electric Support.

    0x1416 (5142)

    Mitop disconnected. Call Schneider Electric support

    Contact Schneider Electric Support.

    0x1402 (5122)

    Current sensor loss. Replace circuit breaker.

    Replace the circuit breaker. Contact Schneider Electric Support.

    0x1403 (5123)

    ENCT disconnected

    Check internal/external wiring of External Neutral Current Transformer (ENCT).

    0x1430 (5168)

    Protection settings reset to factory values

    Update the MicroLogic Active control unit firmware with EcoStruxure Power Commission software. Otherwise, plan to replace the MicroLogic Active control unit.

    0x1409 (5129)

    Unable to read sensor plug

    Check connection of the sensor plug and performer plugs. If the connection is good but the event recurs, replace the sensor plug or the MicroLogic Active control unit.

    0x1518 (5400)

    Self-test 6. Replace control unit.

    Replace the MicroLogic Active control unit. Contact Schneider Electric Support.

    Contact Schneider Electric Support or your Schneider Electric Services representative for more information about who can carry out the recommended actions.

    Resetting a Trip Event

    For information about resetting the circuit breaker after a trip due to an incident detected by the MicroLogic Active self-tests, refer to the relevant document:

    • MasterPacT MTZ1 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

    • MasterPacT MTZ2/MTZ3 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

    Feedback
    QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.