DOCA0265EN-07

Maintenance Menu

Description

The Maintenance menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Tree navigation menu

Maintenance

Assistance

Presents information about the firmware version of the MicroLogic Active control unit.

Health

Describes the health state of the circuit breaker.

Protection Test

Perform a protection test on the MicroLogic Active HMI.

Replacement

Set the circuit breaker information in a replacement MicroLogic Active control unit.

Zigbee

Perform a Zigbee wireless communication test (for certification only).

Assistance

The Assistance menu presents the following data:

Level 3

Level 4

Function description

Assistance

Firmware Version

Displays the MicroLogic Active firmware version in the format aaa.bbb.ccc.

NOTE: The Core Protect Version is also available to view but this is only used when requested by Schneider Electric Customer Care.

Health

The Health menu presents the following data:

Level 3

Level 4

Function description

Health

Contact wear

Displays wear of the contacts as a percentage

Replacement

The Replacement menu presents the following data:

Level 3

Level 4

Level 5

Function description

Replacement

Manuf. Maint

Last manufacturer maintenance

Set the number of months since the last manufacturer maintenance.

Contact Wear

Contact Wear Preset

Set the wear of the contacts as a percentage.

ID

Range

Select the circuit breaker range.

Rating

Select the circuit breaker rating.

Performance

Select the circuit breaker performance.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.