DOCA0265EN-07

Monitoring the Load Profile

Presentation

Seven load profile counters report the number of hours during which the MicroLogic Active control unit has measured current flowing through the circuit breaker, in the following In ratio ranges:

  • Number of hours with current measured below 15 % of the rated current In

  • Number of hours with current measured between 15 and 25% of the rated current In

  • Number of hours with current measured between 26 and 35% of the rated current In

  • Number of hours with current measured between 36 and 50% of the rated current In

  • Number of hours with current measured between 51 and 79% of the rated current In

  • Number of hours with current measured between 80 and 89% of the rated current In

  • Number of hours with current measured at 90% of the rated current In or above

Data Availability

Load profile monitoring data is available with EcoStruxure Power Device app through NFC connection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.