DOCA0265EN-07

Event Display

Introduction

The event status table contains the status of all events at the time of consultation. The status can be inactive, active, or held.

Events which are in the active and held state are displayed on the following interfaces:

  • MicroLogic Active display screen.

  • EcoStruxure Power Commission software.

  • EcoStruxure Power Device app.

The status of an event can be checked using the wired or Zigbee communication network.

Displaying Events on the MicroLogic Active Display Screen

Display the active and held alarm events on the MicroLogic Active display screen from the tree navigation menu, at Alarms/History > Active Alarms.

High and medium severity active and held events are displayed.

If the event is completed, it is moved to Alarms/History > Alarms History.

Displaying Events on EcoStruxure Power Commission Software

High and medium severity, active and held events are displayed.

Events can be sorted by:

  • Date

  • Severity:

    • High severity events

    • Medium severity events

  • History

  • Type

Displaying Events on EcoStruxure Power Device App

By default, events are sorted chronologically. They can be sorted by other parameters such as date, severity, type or history.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.