DOCA0265EN-07

Configuration Menu

Description

The Configuration menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Tree navigation menu

Configuration

General

Settings of the HMI display and control of access to protection settings.

Network

Settings of nominal voltage and frequency, and power sign.

Measures

Settings of measurement calculation.

BCIM

Settings of the BCIM module.

Communication

Settings of communication parameters.

General

The General menu presents the following data:

Level 3

Level 4

Level 5

Function description

General

Language

List of display screen languages.

Date & time

DD/MM/YYY

HH:MM:SS

Set the date format. Available options are:

  • DD/MM/YYYY

  • MM/DD/YYYY

  • YYYY/MM/DD

Set the time.

NOTE: Configuration of the date and time format is protected by the PIN code of the SecurityAdmin account.

Change PIN code

Change the PIN code by using tree navigation mode.

NOTE: Changing the PIN code is protected by the PIN code of the SecurityAdmin account.

Network

The Network menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Network

Voltage

Vn (V)

Rated voltage.

Setting values include: 208 / 220 / 230 / 240 / 380 / 400 / 415 / 440 / 480 / 500 / 525 / 550 / 575 / 600 / 660 / 690 V.

Factory setting = 400.

Frequency

Hz

Rated frequency

  • 50 Hz (factory setting)

  • 60 Hz

Phase Rot.

1,2,3

1,3,2

Power sign

Power flow sign setting:

  • P+ = the active power flows from upstream (top) to downstream (bottom) (factory setting).

  • P– = the active power flows from downstream (bottom) to upstream (top).

VT ratio

VT Primary

VT primary voltage.

Values from 100 to 1,250 V, in increments of 1 V.

VT Secondary

VT secondary voltage.

Values from 100 to 690 V, in increments of 1 V.

Measures

The Measures menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Measures

PF/Var

Sign convention for cos φ, PF power factor, and reactive power:

  • IEC (factory setting)

  • IEEE

System type

Poles Nbr

3P or 4P

ENVT

External neutral voltage tap. Setting values include:

  • If 4P: NO (for display only)

  • If 3P: NO or YES (factory setting)

NOTE: If ENVT setting is NO, the VT ratio sub menu is hidden.

ENCT

External neutral current transformer. Setting values include:

  • If 4P: NO (for display only)

  • If 3P: NO (factory setting) or YES

P Calc

Total power calculation method:

  • Vector

  • Arithmetic (factory setting)

E Calc

Energy Accumulation mode. Energy values to be used in energy calculations:

  • Absolute (factory setting)

  • Signed

BCIM

The BCIM menu presents the following data:

Level 3

Level 4

Level 5

Level 6

Function description

BCIM

BCIM

Configure the presence of the BCIM module in the circuit breaker:

  • No

  • Yes

Coil XF

Enable control of the XF communicating closing voltage release by the BCIM module:

  • No

  • Yes

Coil MX

Enable control of the MX communicating opening voltage release by the BCIM module:

  • No

  • Yes

IO Settings

IO Mode

Disabled

Select this setting to disable the use of the BCIM module IO ports.

Open/Close

Select this setting to enable the use of the BCIM module IO ports to open and close the circuit breaker.

ERMS

Select this setting to enable the use of the BCIM module IO ports to engage and disengage ERMS mode.

Alarms

Select this setting to enable the use of the BCIM module IO ports to signal the status of selected alarms.

IO Channel 1

When IO Mode = Alarms, select one alarm from the list, to be signaled on IO Channel 1.

IO Channel 2

When IO Mode = Alarms, select one alarm from the list, to be signaled on IO Channel 2.

Identification

Displays the hardware and firmware version of the BCIM module.

NOTE: The BCIM configuration factory settings depend on whether the BCIM module and communicating voltage releases are installed in factory or not.

Communication

The Communication menu presents the following data:

Level 3

Level 4

Level 5

Parameter name

Communication

Zigbee

Identification

Displays the Zigbee ID of the MicroLogic Active AP/EP control unit.

Status

Displays the Zigbee connectivity status of the MicroLogic Active AP/EP control unit.

Provides a means to connect the MicroLogic Active AP/EP control unit to a Zigbee network.

Control Mode

Manual

Configure the control mode to block or allow remote control commands.

NOTE: Configuration of the control mode is protected by the PIN code of the SecurityAdmin account.

Auto Local

Auto Remote

Remote Settings

Enable or disable remote setting of the standard protection functions:

  • ON (enable)

  • OFF (disable)

NOTE: Configuration of Remote Settings is protected by the PIN code of the SecurityAdmin account.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.