DOCA0265EN-07

Prepare MasterPacT MTZ Circuit Breaker Before Setting

Preparing Fixed MasterPacT MTZ Circuit Breakers

Step

Action

1

Turn off all power supplying the equipment before working on or inside the equipment.

2

Use a properly rated voltage sensing device to confirm that power is off.

3

Press the opening pushbutton to open the circuit breaker.

4

Check that the position indicators show that the circuit breaker is OFF and that the mechanism is discharged.

Preparing Drawout MasterPacT MTZ Circuit Breakers

DANGER
HAZARD OF DEVICE FALLING
  • Be sure that lifting equipment has lifting capacity for the device being lifted.
  • Follow manufacturer’s instructions for use of lifting equipment.
  • Wear hard hat, safety shoes, and heavy gloves.
Failure to follow these instructions will result in death or serious injury.

Step

Action

1

Turn off all power supplying the equipment before working on or inside the equipment.

2

Use a properly rated voltage sensing device to confirm that power is off.

3

Press the opening pushbutton to open the circuit breaker.

4

Install the circuit breaker in the chassis.

5

Rack-in the circuit breaker in Test position.

6

Check that the position indicators show that the circuit breaker is OFF, in test position, and the mechanism is discharged.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.