DOCA0265EN-07

Energy Reduction Maintenance Settings (ERMS)

Presentation

The ERMS function is used to reduce instantaneous overcurrent protection settings so that the circuit breaker trips as soon as possible when a short circuit occurs. Minimizing the time between short circuit and trip helps to reduce the risk of injury when qualified electrical personnel are near energized equipment.

When the ERMS function is engaged, the ERMS protection settings replace the standard instantaneous overcurrent protection settings.

Availability

The ERMS function is available on MicroLogic Active 2.0, 5.0 and 6.0 control units for IEC standard.

To use the ERMS function with an external selector switch, the optional BCIM module must be installed in the circuit breaker and configured in ERMS mode. See BCIM Module in ERMS Mode.

Operating Principle

The ERMS function can be engaged or disengaged by using the ERMS button, or by using an external selector switch connected to the BCIM module.

While the ERMS function is engaged:

  • The ERMS LED (A) is lit in blue.

  • The LSIG home screen is blue.

  • The Quick View screens are blue.

  • All other screens are not blue.

Use-case Examples

The conditions of operation of electrical installations are specified by national regulations (for example, NPFA70E for USA, EN 50110 for Europe). These regulations require an assessment of electrical risk before carrying out any operation. The assessment must specify when the ERMS function should be implemented and engaged.

Whenever possible the electrical installation should be de-energized. When working in the vicinity of live parts without all doors or panels of the switchboard closed and secured, the ERMS function can be engaged to reduce the consequences of a short circuit. A risk assessment specific to each situation must be carried out, even when the ERMS function is used.

The following table gives examples of use-cases inside or close to a switchboard, where engaging the ERMS function is recommended. The recommendations are based on the assumptions that:

  • The ERMS function is embedded in the upstream device on the supply side of the switchboard in question.

  • The switchboard has only one supply.

Operation

Location

Addition of device in spare slot in the switchboard

Inside switchboard

Thermal inspection

Inside switchboard

Measurement reading inside switchboard, requiring opening of door or panels

Inside switchboard

Measurement with portable equipment (for example, voltage presence, phase rotation, power quality)

Inside switchboard

First energization or re-energization of the equipment

In electrical room, less than 0.3 m (12 in) from switchboard

Device unlocking with padlock or key

In electrical room, less than 0.3 m (12 in) from switchboard

Device closing

In electrical room, less than 0.3 m (12 in) from switchboard

Engaging the ERMS Function

DANGER
hazard of incorrect ERMS status
  • Do not rely on the ERMS status signaled on the BCIM IO port.
  • Use the blue ERMS LED on the MicroLogic Active control unit to check ERMS status before working on or inside the equipment.
Failure to follow these instructions will result in death or serious injury.

The ERMS function can be engaged:

Disengaging the ERMS Function

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Prior to disengaging ERMS:
  • Carefully inspect your work area, and remove any tools and objects left inside the equipment.
  • Ensure that all personnel are away from the equipment, and devices, doors, and covers are in place.
Failure to follow these instructions will result in death or serious injury.

The ERMS function must be disengaged by the interface that engaged it:

  • If it is engaged by the ERMS button, it must be disengaged by the ERMS button. See Disengaging the ERMS Function.

  • If it is engaged by the external selector switch connected to the BCIM module, it must be disengaged by the external selector switch.

BCIM Module in ERMS Mode

When configured in ERMS mode, the optional BCIM module can be used with an external lockable selector switch to engage or disengage the ERMS function.

The BCIM module is equipped with:

  • An input connected to the ERMS selector switch, with the following characteristics:

    • When the input is energized, the ERMS function is disengaged.

    • When the input is not energized, the ERMS function is engaged.

  • An output to activate an external pilot light when the ERMS function is engaged.

The ERMS function is engaged by turning the external selector switch.

To configure the BCIM module in ERMS mode, set the BCIM parameters on the MicroLogic Active display screen, from the tree navigation menu at Configuration > BCIM as follows:

  • BCIM = Yes

  • IO Settings > IO Mode = ERMS

The other BCIM parameters have no impact on the ERMS function.

For more information, refer to BCIM configuration.

ERMS Settings

When the ERMS function is engaged, the standard setting for instantaneous overcurrent protection is overridden by the default ERMS setting for instantaneous overcurrent protection:

Protection function

Setting

Unit

Default ERMS value

MicroLogic Active type

Instantaneous overcurrent protection

Ii

A

2.0 x In

MicroLogic Active 5.0 and 6.0

1.5 x Ir

MicroLogic Active 2.0

The default ERMS setting for instantaneous overcurrent protection cannot be modified.

The other protection functions use standard protection settings.

Predefined Events

The function generates the following predefined events:

Code

Event

History

Severity

0x0C03 (3075)

ERMS engaged

Protection

Low

Predefined events cannot be modified by the user. For general information about events, refer to Event management.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.