DOCA0265EN-07

Quick View Mode

Quick View

Quick view presents a sequence of screens, depending on the type of MicroLogic Active control unit. The screens display a snapshot of the status and operating values of the control unit. The values shown on the protection screens are the active protection settings currently used by the protection functions.

The active protection settings are:

  • Standard protection settings, by default.

  • ERMS protection settings, when ERMS is engaged.

  • Fallback protection settings, when the MicroLogic Active control unit reverts to fallback protection settings after the event Last protection settings have not been applied. (code 0x142F).

The following is an example of the Quick View screens for the MicroLogic Active 6.0 control unit when standard protection settings are active.

List of Quick View Screens

Depending on the type of the MicroLogic Active control unit, Quick View displays the following screens:

Screen

Description

MicroLogic Active type

Health(1)

Displays the health state of the circuit breaker:

MicroLogic Active 2.0, 5.0 and 6.0
 

Good health state (green)

 
 

Medium-severity detected alarm that requires an action to be planned (orange)

 
 

High-severity detected alarm that requires immediate action (red)

 

Current(1)

Displays I1, I2, I3 RMS current on phase 1, 2, 3 values as bar graphs expressed in % of Ir.The three current values are displayed in Amps under the bar graph.

MicroLogic Active 2.0, 5.0 and 6.0

Trip Curve

Displays the message:

  • Standard protection LSIG settings, by default.

  • ERMS protection LSIG settings, when ERMS is engaged.

  • Fallback protection LSIG settings, when fallback settings are in use.

MicroLogic Active 2.0, 5.0 and 6.0

LI settings

Displays a selection of active protection settings:

  • Long time overcurrent protection threshold Ir

  • Long time overcurrent protection time delay tr

  • Instantaneous overcurrent protection threshold Ii

MicroLogic Active 2.0

LSI settings

Displays a selection of active protection settings:

  • Long time overcurrent protection threshold Ir

  • Long time overcurrent protection time delay tr

  • Short time overcurrent protection threshold Isd

  • Short time overcurrent protection time delay tsd

  • Instantaneous overcurrent protection threshold Ii

MicroLogic Active 5.0

LSIG settings

Displays a selection of active protection settings:

  • Long time overcurrent protection threshold Ir

  • Long time overcurrent protection time delay tr

  • Short time overcurrent protection threshold Isd

  • Short time overcurrent protection time delay tsd

  • Instantaneous overcurrent protection threshold Ii

  • Ground- fault protection threshold Ig

  • Ground- fault protection time delay tg

MicroLogic Active 6.0

(1) Screen data is refreshed every second.

NOTE: When ERMS is engaged, the Quick View screens are blue.

Starting Quick View Scrolling

Quick View scrolling starts automatically after 3 minutes of inactivity on the MicroLogic Active control unit keypad, as long as there is no pending user action.

The display scrolls through a selection of screens in a repeated loop. Each screen is displayed for 5 seconds before the next screen is displayed.

Stopping Quick View Scrolling

Stop Quick View scrolling by pressing the Back button. The LSIG home screen is displayed.

When the MicroLogic Active control unit detects any of the following events, Quick View scrolling is interrupted and a pop-up message is displayed:

  • Trip

  • High severity alarm

  • Medium severity alarm

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.