DOCA0265EN-07

Monitoring the Circuit Breaker

Presentation

The monitoring of the circuit breaker consists in monitoring its ability to establish or interrupt a circuit and to provide protection against electrical faults. The MicroLogic Active control unit therefore monitors:

When the MicroLogic Active control unit detects an incident in one of the monitored functions listed, an event is generated with an orange or red pop-up screen and corresponding event message.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.