DOCA0265EN-07

MicroLogic Active E/EP/Ei Energy Metering

Presentation

The MicroLogic Active E/EP/Ei control unit calculates the different types of energy using energy meters and provides the values of:

  • The total active energy Ep, the active energy delivered (into the load) Ep delivered, and the active energy received (out of the load) Ep received

  • The active energy for each phase delivered (into the load): Ep1 delivered, Ep2 delivered and Ep3 delivered

  • The active energy for each phase received (out of the load): Ep1 received, Ep2 received and Ep3 received

  • The total reactive energy Eq, the reactive energy delivered (into the load) Eq delivered, and the reactive energy received (out of the load) Eq received

  • The reactive energy for each phase delivered (into the load): Eq1 delivered, Eq2 delivered and Eq3 delivered

  • The reactive energy for each phase received (out of the load): Eq1 received, Eq2 received and Eq3 received

  • The total apparent energy Es

  • The apparent energy for each phase Es1, Es2 and Es3

The energy values are calculated every second, and shown as an hourly consumption. Values are stored in non-volatile memory every hour.

A resettable counter is available for each energy meter.

NOTE: To perform reliable energy measurement across the current range the control unit must be powered by an external 24 Vdc power supply.

Principle of Energy Calculation

By definition energy is the integration of the real-time power over a period T. The integration period T lasts for a number of cycles equal to the rated frequency.

Partial Energy Meters

For each type of energy, active or reactive, a partial received energy meter and a partial delivered energy meter calculate the accumulated energy by incrementing once a second:

  • Delivered energy is always counted positively.

    Edelivered(t) = Edelivered(t - 1) + (Gdelivered(t))/3600

    where Gdelivered = Ptot or Qtot > 0

  • Received energy is always counted negatively.

    Ereceived(t) = Ereceived(t - 1) + (|Greceived(t)|)/3600

    where Greceived = Ptot or Qtot < 0

Energy Meters

From the partial energy meters and for each type of energy, active or reactive, an energy meter provides either of the following measurements once a second:

  • The absolute energy, by adding the received and delivered energies together. The energy accumulation mode is absolute.

  • The signed energy, by differentiating between received and delivered energies. The energy accumulation mode is signed.

The apparent energy Es is always counted positively.

Selecting Energy Calculation

The information sought determines calculation selection:

  • The absolute value of the energy that has crossed the poles of a circuit breaker or the cables of an item of electrical equipment is relevant for maintenance of an installation.

  • The signed values of the energy delivered and the energy received are required to calculate the economic cost of an item of equipment.

By default, absolute energy accumulation mode is configured.

Select the energy calculation mode on the MicroLogic Active E/EP/Ei display screen, from the tree navigation menu, at Configuration > Measures > E calcul.

Resetting Energy Meters

The energy meters can be reset as follows:

  • On the MicroLogic Active E/EP/Ei display screen, from the tree navigation menu, at Measures > Energy > Reset Counters.

  • By sending a command using the wired communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.