DOCA0265EN-07

Standard Protection Setting Procedure

Standard Protection Setting Session

The procedure for setting a standard protection function conforms to UL489SE, with an exclusive editing session and a two-step procedure for submitting and applying standard protection setting changes.

Access to the protection function is protected by a PIN code.

The standard protection functions are:

  • Long time overcurrent protection

  • Short time overcurrent protection

  • Instantaneous time overcurrent protection

  • Ground fault protection

  • Neutral protection

Two modes of protection setting are available:

  • Quick settings mode

  • Fine adjustment mode

The availability of the setting modes depends on the type of standard protection setting, described in Standard Protection Functions.

If the MicroLogic Active control unit power supply is interrupted, use the Mobile Power Pack to enable the protection setting procedure on the MicroLogic Active HMI.

Setting Protection Using Quick Setting Mode

The following example shows how to set the ground fault protection using quick setting mode:

Step

Action

Screen

1

Use a flat screwdriver to break the seal and lift the cover of the protection settings button.

  • Press the protection settings button.

  • Press OK.

NOTE: Press the protection settings button at any time during the following procedure if you want to cancel the settings and exit the Standard Settings menu.

2

If a SecurityAdmin account has been created, the PIN code menu opens.

If a SecurityAdmin account has not been created, see Setting the PIN Code.

3

Enter the PIN code as follows:

  • Press the up and down buttons to increment or decrement the selected digit by one.
  • Press OK to confirm the current digit value, and move to the next digit on the right.
  • Press Back to go back to the previous digit on the left.

4

Press OK on the right-most digit to confirm the PIN code and enter the editing session.

NOTE: After 5 minutes of inactivity, the editing session closes and the display reverts to the LSIG home screen.

5

The Standard Settings menu opens.

  • Each standard protection function is represented by a label with a single letter (L, S, I , G or N) on a grey background.

  • The grey background indicates that parameters are editable.

  • Parameters for each protection function are displayed next to the label.

  • A parameter displayed on a grey background indicates that the parameter is selected for editing.

6

Press the down button to select the I²t and tg parameters in the G area.

7

Press OK to edit the I²t parameter.

8

The I²t setting menu is displayed. In the example,I²t OFF is selected.

9

Press the up button to select I²t ON.

Press OK to confirm selection of I²t ON, and to edit the tg parameter.

10

The Ground fault tg quick setting menu is displayed.

NOTE: If both setting modes are available for the selected protection setting, the Setting Mode menu opens, and you have to select Quick setting mode.

11

Press the up and down buttons to scroll through available settings.

Press OK to confirm the new setting.

12

The Standard Settings menu is displayed. Parameter settings which have been modified but not applied, are displayed in yellow.

13

Use the up, down and OK buttons to select the next parameter to edit, and repeat from step 8.

14

To apply the new settings, use the down button to scroll to Apply settings.

15

Press OK to apply the new settings.

The Apply settings menu opens.

16

Use the down button to do one of the following:

  • Scroll down to Confirm, and press OK to confirm that you want to apply the new settings.

  • Scroll down to Discard, and press OK to confirm that you want to discard the new settings.

17

If you selected Confirm in step 17, after a delay, the screen displays the LSIG home screen with the new settings.

18

If you selected Discard in step 17, the screen displays a confirmation menu asking you to confirm that you want to exit settings.

Do one of the following:

  • Press OK to confirm that you want to exit settings. You return to the screen from which the request was initially made.

  • Use the down button to scroll down to Cancel and press OK to continue editing. This takes you back to step 13.

19

Close and seal the cover of the protection settings button.

Setting Protection Using Fine Adjustment Mode

The following example shows how to set the long-time overcurrent protection using fine adjustment mode:

Step

Action

Screen

1

Use a flat screwdriver to break the seal and lift the cover of the protection settings button.

  • Press the protection settings button.

  • Press OK.

NOTE: Press the protection settings button at any time during the following procedure if you want to cancel the settings and exit the Standard Settings menu.

2

If a SecurityAdmin account has been created, the PIN code menu opens.

If a SecurityAdmin account has not been created, see Setting the PIN Code.

3

Enter the PIN code as follows:

  • Press the up and down buttons to increment or decrement the selected digit by one.
  • Press OK to confirm the current digit value, and move to the next digit on the right.
  • Press Back to go back to the previous digit on the left.

4

Press OK on the right-most digit to confirm the PIN code and enter the editing session.

NOTE: After 5 minutes of inactivity, the editing session closes and the display reverts to the LSIG home screen.

5

The Standard Settings menu opens.

  • Each standard protection function is represented by a label with a single letter (L, S, I , G or N) on a grey background.

  • The grey background indicates that parameters are editable.

  • Parameters for each protection function are displayed next to the label.

  • A parameter displayed on a grey background indicates that the parameter is selected for editing.

6

In the example, the Ir parameter in the L (long-time overcurrent protection settings) area is selected for editing.

7

Press OK to edit the Ir parameter. The setting mode menu opens.

Press the down button to select Fine adjustment mode.

NOTE: If only one setting mode is available for the selected protection setting, the setting mode menu will not open. Instead, the selected protection setting menu will open.

8

Press OK.

The Long time Ir fine adjustment menu is displayed, with the cursor over the first digit.

The first digit is displayed in white to indicate that it is selected for editing.

9

Press the up and down buttons to increment or decrement the selected digit by one.

  • Press OK to confirm the current digit value, and move to the next digit on the right.

  • Press Back to go back to the previous digit on the left.

10

Press OK on the right-most digit to confirm the new parameter setting.

11

The Standard Settings menu is displayed. Parameter settings which have been modified but not applied, are displayed in yellow.

12

Use the up, down and OK buttons to select the next parameter to edit, and repeat from step 9.

13

To apply the new settings, use the down button to scroll to Apply settings.

14

Press OK to apply the new settings.

The Apply settings confirmation menu opens.

15

Use the down button to do one of the following:

  • Scroll down to Confirm, and press OK to confirm that you want to apply the new settings.

  • Scroll down to Discard, and press OK to confirm that you want to discard the new settings.

16

If you selected Confirm in step 16, after a delay, the screen displays the LSIG home screen with the new settings.

17

If you selected Discard in step 16, the screen displays a confirmation menu asking you to confirm that you want to exit settings.

Do one of the following:

  • Press OK to confirm that you want to exit settings. You return to the screen from which the request was initially made.

  • Use the down button to scroll down to Cancel and press OK to continue editing. This takes you back to step 12.

18

Close and seal the cover of the protection settings button.

Pop-up Notices

The following table indicates the necessary action to take if a pop-up notice is displayed while editing a protection setting:

Message

Description

Action

Access denied. Another session already opened

You cannot open an editing session to set protection settings because a session is open on another interface.

Protection settings are for display only, and can be consulted on the Protection menu in tree navigation mode. It is not possible to set settings as long as a session is open on another interface. Try again later.

Press OK to acknowledge the message and return to the LSIG home screen

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.