DOCA0265EN-07

Assistance

Presentation

The assistance menu on the MicroLogic Active display screen gives information about the firmware version of the microprocessors installed in the MicroLogic Active control unit. Firmware updates are managed with EcoStruxure Power Commission software.

Data Availability

The firmware version is available as follows:

  • On the MicroLogic Active display screen, from the tree navigation menu, at: Maintenance > Assistance > Firmware version

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

  • On a server or remote controller using the wired communication network

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.