DOCA0265EN-07

HMI Display Modes

Presentation

The MicroLogic Active control unit HMI supports the following display modes:

  • Quick View mode to display a selection of screens

  • Tree Navigation mode to access all screens through a menu structure

NOTE: Both Quick View and Tree Navigation display modes are overridden by event messages.

Quick View Mode

Quick View mode is activated after 3 minutes of inactivity on the MicroLogic Active control unit keypad.

In Quick View mode the display scrolls through a selection of screens in a repeated loop.

Tree Navigation Mode

In Tree Navigation display mode, use the navigation buttons to navigate the menu structure. Tree Navigation display mode presents a single network of menus, with monitoring values and editable configuration settings.

Tree navigation is accessible from the LSIG home screen by pressing one of the navigation buttons, OK, Back, Up, or Down.

Refer to the MicroLogic Active local HMI description for information about how to use the HMI buttons to:

  • Navigate the menu structure

  • Access and edit settings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.