DOCA0265EN-07

Date and Time

Presentation

MicroLogic Active date and time are used for time stamping events to provide a chronological order.

The date and time of the MicroLogic Active control unit and the other ULP modules (BCIM module, EIFE or IFM interface) of the intelligent modular unit (IMU) are synchronized. Setting the date and time of one module sets the date and time of all the modules of the IMU.

NOTE: The date and time of MicroLogic Active and other ULP modules are automatically reset to default value for the date (Jan 01 2000) when the internal battery of the MicroLogic Active control unit is removed and the control unit has no other power supply.

Setting the Date and Time Manually

MicroLogic Active date and time can be set manually:

  • On the MicroLogic Active display screen, from the tree navigation menu, at Configuration > General > Date & Time.

  • With a web browser connected to the IFM or EIFE webpage.

Predefined Events

The following event is generated when date and time are set manually:

Code

Event

History

Severity

0x1107 (4359)

Date and time set

Operation

Low

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.