DOCA0265EN-07

Obtain Data from MicroLogic Active Control Unit

The settings can be retrieved from the MicroLogic Active control unit, by manually noting the settings displayed:

  • On the MicroLogic Active HMI

  • In EcoStruxure Power Device app

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.