DOCA0265EN-07

Instantaneous Overcurrent Protection (I or ANSI 50)

Presentation

Instantaneous protection helps to protect equipment against phase-to-phase, phase-to-neutral and phase-to-ground short circuits. The protection operates with a definite time characteristic. It trips without additional time delay as soon as the setting current is exceeded.

The protection offers two tripping modes, with different breaking times:

  • Standard mode (when ERMS is not engaged): breaking time of 50 ms, used for applications requiring selectivity. Full selectivity can be provided with any ComPacT NSX or PowerPacT H-, J-, L-frame circuit breaker installed downstream of a MasterPacT MTZ circuit breaker (Refer to selectivity tables for details for Ue ≤ 440 Vac).

  • Fast mode (when ERMS is engaged): breaking time of 30 ms, typically used for applications where the thermal constraints of the equipment need to be limited and when selectivity is not required. For more information, refer to LVPED318033EN Complementary Technical Information.

NOTE: On MicroLogic Active 2.0, instantaneous protection is based on short-time protection without time setting with standard breaking time of 80 ms.

Availability

Instantaneous overcurrent protection is available on:

  • MicroLogic Active 2.0, 5.0 and 6.0 control units for IEC standard

  • 3-pole and 4-pole circuit breakers

It is powered by the current flowing through the internal current transformers of the circuit breaker and it does not require an additional external power supply.

Operating Principle

The instantaneous overcurrent protection threshold sets the level of short-circuit current at which the circuit breaker trips with no intentional time delay.

For MicroLogic Active 5.0 and 6.0 control units for IEC standard, instantaneous overcurrent protection can be disabled.

For MicroLogic Active 2.0 control units for IEC standard, instantaneous overcurrent protection cannot be disabled.

Instantaneous overcurrent protection overrides short-time overcurrent protection when the instantaneous overcurrent threshold is adjusted to the same or a lower setting than the short-time overcurrent threshold.

Setting the Protection for MicroLogic Active 2.0

The instantaneous overcurrent protection setting is Ii: instantaneous overcurrent protection threshold (corresponds to a short-time overcurrent protection threshold without time setting).

Two modes of configuring the protection settings are available:

  • Quick setting mode is used to configure quick protection settings

  • Fine adjustment mode is used to configure fine protection settings

Quick Protection Settings for MicroLogic Active 2.0

Quick protection settings are available:

Setting

Unit

Values

Factory setting

Ii

A

OFF, (1.5 / 2 / 2.5 / 3 / 4 / 5 / 6 / 8 / 10) x Ir

1.5 x Ir

For more information, refer to the setting guidelines.

Fine Protection Settings for MicroLogic Active 2.0

Fine protection settings are available:

  • In fine adjustment mode, on the MicroLogic Active HMI

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

Setting

Unit

Range

Step

Factory setting

Ii

A

1.5–10 x Ir

0.1 x Ir

1.5 x Ir

For more information, refer to the setting guidelines.

Protection Characteristics for MicroLogic Active 2.0

Characteristic

Unit

Standard value

ERMS value

Breaktime at 2 x Ii threshold

ms

≤ 80

≤ 80

Non-tripping time

ms

> 20

> 20

Accuracy on threshold

%

+/- 10

+/- 10

Setting the Protection for MicroLogic Active 5.0 and 6.0

Instantaneous overcurrent protection for MicroLogic Active 5.0 and 6.0 can be enabled or disabled with EcoStruxure Power Commission software.

The instantaneous overcurrent protection setting is Ii: instantaneous overcurrent protection threshold.

Two modes of configuring the protection settings are available:

  • Quick setting mode is used to configure quick protection settings

  • Fine adjustment mode is used to configure fine protection settings

Quick Protection Settings for MicroLogic Active 5.0 and 6.0

Quick protection settings are available:

Setting

Unit

Values

Factory setting

Ii

A

OFF, (2 / 3 / 4 /6 / 8 / 10 / 12 / 15) x In

2 x In

For more information, refer to the setting guidelines.

Fine Protection Settings for MicroLogic Active 5.0 and 6.0

Fine protection settings are available:

  • In fine adjustment mode, on the MicroLogic Active HMI

  • With EcoStruxure Power Commission software

  • With EcoStruxure Power Device app

Setting

Unit

Range

Step

Factory setting

Ii

A

2.0–15 x In

0.1 x In

2.0 x In

For more information, refer to the setting guidelines.

Protection Characteristics for MicroLogic Active 5.0 and 6.0

Characteristic

Unit

Standard value

ERMS value

Breaktime at 2 x threshold

ms

≤ 50

≤ 30

Non-tripping time

ms

> 20

0

Accuracy on threshold

%

+/- 10

+/- 10

Predefined Events for MicroLogic Active 2.0, 5.0 and 6.0

The protection function generates the following predefined events:

Code

Event

History

Severity

0x4002 (16386)

Instantaneous (Ii) trip

Trip

High

Predefined events cannot be modified by the user. For general information about events, refer to Event management.

The trip event is generated when the circuit breaker tripping voltage release (MITOP) activates.

Predefined Events for MicroLogic Active 5.0 and 6.0

When instantaneous overcurrent protection is disabled, the following event is generated:

Code

Event

History

Severity

0x0C08 (3080)

Ii protection disabled

Protection

Low

Recommended Actions

Code

Event

Recommended actions

0x4002 (16386)

Instantaneous (Ii) trip

Reset the circuit breaker. See Resetting a Trip Event.

0x0C08 (3080)

Ii protection disabled

No action required. For information only.

Protection Test for MicroLogic Active 2.0 and 5.0

The protection test function for MicroLogic Active 2.0 and 5.0 control units simulates a trip generated by instantaneous overcurrent protection.

Perform the protection test as follows:

Step

Action

1

Check that the circuit breaker is closed and the control unit is supplied with power (ready LED is flashing).

2

Use the MicroLogic Active HMI to perform the protection test.

The Ii test button pressed event is generated.

3

The circuit breaker trips.

The Ii test trip event is generated.

4

If the circuit breaker does not trip, the Ii test - no trip event is generated.

Restart the test. If the circuit breaker does not trip again, contact your Schneider Electric Services representative.

Protection Test Events for MicroLogic Active 2.0 and 5.0

The protection test function generates the following predefined events:

Code

Event

History

Severity

0x4035 (16437)

Ii test trip

Trip

High

0x151B (5403)

Ii test - no trip

Diagnostic

High

0x151C (5404)

Ii test button pressed

Diagnostic

Low

Recommended Actions for MicroLogic Active 2.0 and 5.0 Protection Test

Code

Event

Recommended actions

0x4035 (16437)

Ii test trip

Reset the circuit breaker. See Resetting a Trip Event.

0x151B (5403)

Ii test - no trip

Restart the test. If the circuit breaker does not trip again, contact your Schneider Electric Services representative.

0x151C (5404)

Ii test button pressed

No action required. For information only.

Resetting a Trip Event

For information about resetting the circuit breaker after a trip due to an electrical fault, refer to the relevant document:

  • MasterPacT MTZ1 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

  • MasterPacT MTZ2/MTZ3 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.