DOCA0265EN-07

About the Document

Document Scope

The aim of this guide is to provide users, installers, and maintenance personnel with the technical information needed to operate MicroLogic Active control units in MasterPacT MTZ circuit breakers.

This guide applies to the following MicroLogic Active control units for IEC standard:

  • MicroLogic Active 2.0 A, 5.0 A, 6.0 A

  • MicroLogic Active 2.0 AP, 5.0 AP, 6.0 AP

  • MicroLogic Active 2.0 E, 5.0 E, 6.0 E

  • MicroLogic Active 2.0 EP, 5.0 EP, 6.0 EP

  • MicroLogic Active 6.0 Ei

NOTE: A MicroLogic Active 6.0 Ei control unit is a MicroLogic Active 6.0 E control unit without NFC wireless communication capability.

All the information related to MicroLogic Active 6.0 E control units presented in this guide applies to MicroLogic Active 6.0 Ei control units, except information about NFC wireless communication.

Validity Note

This guide applies to MicroLogic Active control units with firmware version 004.004.000 or greater.

Online Information

The characteristics of the products described in this document are intended to match the characteristics that are available on www.se.com. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.se.com, consider www.se.com to contain the latest information.

Product Related Information

WARNING
hazard of electric shock
Do not use MasterPacT MTZ circuit breakers with MicroLogic Active control units:
  • On power systems with IT grounding system with voltage above 600 Vac.
  • On power systems with other grounding system with voltage above 690 Vac.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
hazard of burns
Apply appropriate personal protective equipment (PPE) when the MasterPacT MTZ circuit breaker ambient temperature is above 50 °C (122 °F).
Failure to follow these instructions can result in injury or equipment damage.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords and PIN codes at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

For information about cybersecurity for MicroLogic Active control unit refer to Cybersecurity Recommendations and DOCA0122•• MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide.

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

Related Documents for IEC Devices

Title of documentation Reference number

MasterPacT MTZ with MicroLogic Active Control Unit - Catalog

LVPED225010EN

MasterPacT MTZ1 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

DOCA0284EN
DOCA0284ES
DOCA0284ZH

MasterPacT MTZ1 - Fixed IEC Circuit Breaker with MicroLogic Active Control Unit - Instruction Sheet

PKR4242702

MasterPacT MTZ1 - Drawout IEC Circuit Breaker with MicroLogic Active Control Unit - Instruction Sheet

PKR4242802

MasterPacT MTZ2/MTZ3 IEC Circuit Breakers with MicroLogic Active Control Unit - User Guide

DOCA0285EN
DOCA0285ES
DOCA0285ZH

MasterPacT MTZ2/MTZ3 - Fixed IEC Circuit Breaker with MicroLogic Active Control Unit - Instruction Sheet

PKR4242002

MasterPacT MTZ2/MTZ3 - Drawout IEC Circuit Breaker with MicroLogic Active Control Unit - Instruction Sheet

PKR4243502

Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - User Guide

DOCA0387EN
DOCA0387ES
DOCA0387ZH

MasterPacT MTZ IEC Circuit Breakers with MicroLogic Active Control Unit - Maintenance Guide

DOCA0305EN
DOCA0305ES
DOCA0305ZH

MasterPacT MTZ IEC Circuit Breakers with MicroLogic Active Control Unit - End-User Maintenance Procedures

DOCA0306EN
DOCA0306ES
DOCA0306ZH

MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

DOCA0384EN
DOCA0384ES
DOCA0384FR
DOCA0384ZH

MasterPacT MTZ - MicroLogic Active Control Unit - Firmware Release Notes

DOCA0267EN

MicroLogic Trip Units and Control Units - Firmware History

DOCA0155EN

Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - Firmware Release Notes

DOCA0395EN

MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

DOCA0122EN
DOCA0122ES
DOCA0122FR
DOCA0122ZH

ULP (Universal Logic Plug) System - User Guide

DOCA0093EN
DOCA0093ES
DOCA0093FR
DOCA0093ZH

Enerlin'X IFE - Ethernet Switchboard Server - User Guide

DOCA0084EN
DOCA0084ES
DOCA0084FR
DOCA0084ZH

Enerlin'X IFE - Ethernet Interface for One Circuit Breaker - User Guide

DOCA0142EN
DOCA0142ES
DOCA0142FR
DOCA0142ZH

Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

DOCA0106EN
DOCA0106ES
DOCA0106FR
DOCA0106ZH

EcoStruxure Panel Server - User Guide

DOCA0172EN
DOCA0172ES
DOCA0172FR
DOCA0172DE
DOCA0172IT
DOCA0172PT

You can download these technical publications and other technical information from our website at www.se.com/ww/en/download/.

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.