DOCA0265EN-07

Event Definition

Definition

An event is a change in state of digital data, or any incident detected by the MicroLogic Active control unit or EIFE Ethernet interface.

Events are time stamped and logged in the event history of each module.

Events are categorized according to a level of severity:

  • High: urgent corrective action is required.

  • Medium: corrective action needs to be scheduled.

  • Low: for information only.

All high and medium severity events generate an alarm and a pop-up notification screen on the MicroLogic Active control unit display screen.

Low severity events are information-type events. They can be consulted with EcoStruxure Power Commission software.

Alarms and trips are events that require specific attention from the user:

  • A trip is a high severity event generated when the circuit breaker trips.

  • An alarm is an event with medium or high severity.

The information in this part is valid for events detected by the MicroLogic Active control unit.

For information about EIFE events, refer to DOCA0106•• Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide.

Management of Events by MicroLogic Active Control Unit

The following diagram gives an overview of how events are managed by the MicroLogic Active control unit.

Event Time Stamping

Each event is time stamped with the date and time of the MicroLogic Active internal clock.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.