DOCA0265EN-07

Presentation

MicroLogic Active Control Units for IEC Standard - Overview

MasterPacT MTZ circuit breakers with MicroLogic Active control units provide functions of protection, metering, diagnostics and communication.

MicroLogic Active control units allow local operation and monitoring of MasterPacT MTZ circuit breakers.

The MicroLogic Active control units for IEC standard are:

  • With NFC wireless communication and without Zigbee wireless communication:

    • MicroLogic Active 2.0 A, 5.0 A, 6.0 A

    • MicroLogic Active 2.0 E, 5.0 E, 6.0 E

  • With NFC and Zigbee wireless communication:

    • MicroLogic Active 2.0 AP, 5.0 AP, 6.0 AP

    • MicroLogic Active 2.0 EP, 5.0 EP, 6.0 EP

  • Without wireless communication: MicroLogic Active 6.0 Ei

Convention

For this guide, electrical phases are described as phase 1, phase 2, phase 3 and cover the IEC standard.

Range of MicroLogic Active Control Units for IEC Standard

The following table indicates the standard functions available on MasterPacT MTZ circuit breakers with MicroLogic Active control units for IEC standard:

Function

MicroLogic Active 2.0 A/AP

MicroLogic Active 5.0 A/AP

MicroLogic Active 6.0 A/AP

MicroLogic Active 2.0 E/EP

MicroLogic Active 5.0 E/EP

MicroLogic Active 6.0 E/EP/Ei

Commercial reference

LV933071/LV933071W

LV933072/LV933072W

LV933073/LV933073W

LV947600/LV947600W

LV947602/LV947602W

LV947603/LV947603W/LV949603

Long-time overcurrent protection (L)

Short-time overcurrent protection (S)

Instantaneous overcurrent protection (I)

Ground-fault protection (G)

Neutral protection

Undervoltage protection

Overvoltage protection

Overcurrent and trip cause indicators

Zone selective interlocking

Trip history

Setting change traceability

Current metering

Voltage, power and energy metering

Embedded diagnostics

NOTE: The commercial reference is printed on the front face of the MicroLogic Active control unit and also identifies the standard.

MicroLogic Active Replacement

MicroLogic Active control units can be replaced on site.

For more information, refer to MicroLogic Active Replacement.

Communication Availability

MicroLogic Active control units support wired and wireless communication.

Communication type

MicroLogic Active 6.0 Ei

MicroLogic Active A/E

MicroLogic Active AP/EP

Wireless communication via NFC connection

Wireless communication via Zigbee connection

Wired communication via the USB-C port

Wired communication via the ULP system, by using the optional BCIM module

Wired Communication

MicroLogic Active control units support local and remote wired communication.

Local wired communication is enabled by connection via the USB-C port to:

  • An Android smartphone running the EcoStruxure Power Device app through USB OTG connection

  • A PC running EcoStruxure Power Commission software

Remote wired communication is enabled by using the optional BCIM module connected via the ULP system to:

  • An Ethernet communication network with Modbus TCP/IP protocol

  • A Serial Line communication network with Modbus-SL protocol

The following diagram shows examples of how MicroLogic Active control units communicate within a wired digital system:


Ethernet

USB connection

USB OTG connection

  1. FDM121 display

  2. ULP port module

  3. MasterPacT MTZ2 drawout circuit breaker

  4. MicroLogic Active control unit with BCIM module

  5. Go2SE landing page

  6. EIFE interface

  7. EcoStruxure Power Device app through USB OTG connection

  8. EcoStruxure Power Commission software through USB-C connection

  9. IFE interface

  10. COM terminal block

  11. MasterPacT MTZ2 circuit breaker

  12. Panel Server

  13. IFM interface
  14. MasterPacT MTZ1 circuit breaker

  15. Panel Server, EIFE or IFE webpages

Wireless Communication

In addition to wired communication, MicroLogic Active control units support local wireless communication.

NOTE: Wireless communication is not available with MicroLogic Active 6.0 Ei control unit.

Local wireless communication includes:

The following diagram shows an example of how MicroLogic Active control units communicate within a wireless digital system:

Ethernet

Zigbee wireless communication

A MicroLogic Active control unit

B Go2SE landing page

C EcoStruxure Power Device app through NFC wireless communication

D Panel Server through Zigbee wireless communication, for MicroLogic Active AP/EP control units only

E POI Plus, industrial workstation with energy management software

F EcoStruxure Power Operation (PO) software

G EcoStruxure Power Monitoring Expert (PME) software

H Panel Server webpages

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.