DOCA0265EN-07

Maintenance Schedule

@TW: topic shared between DOCA0305 Maintenance Guide, DOCA0306 End-user Procedures, DOCA0307 Manufacturer Procedures and DOCA0265 Mic Active User Guide

Overview

The MicroLogic Active control unit provides information to help with scheduling preventive maintenance operations.

It monitors maintenance programs performed and generates an event to indicate that Manufacturer maintenance is due.

Operating Principle

The MicroLogic Active control unit generates an event to indicate that Manufacturer maintenance is due.

Manufacturer maintenance schedule events are calculated from the assembly date of the circuit breaker.

Predefined Events

The maintenance schedule function generates the following events:

Code

Event

History

Severity

0x1482 (5250)

Sched. Manufact. maintenance within 3 months

Diagnostic

Medium

Recommended Actions

Code

Event

Recommended actions

0x1482 (5250)

Sched. Manufact. maintenance within 3 months

Plan to schedule the Manufacturer preventive maintenance program within three months. To plan, edit report and track maintenance intervention, you may use EcoStruxure Facility Expert app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.