DOCA0265EN-07

EcoStruxure Power Commission Software

@TW: topic used in DOCA0265 Mic Active user guide and in DOCA0387 BCIM user guide

Overview

EcoStruxure Power Commission software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.

EcoStruxure Power Commission software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

EcoStruxure Power Commission software enables the configuration of MasterPacT MTZ circuit breakers with MicroLogic Active control unit.

For more information, refer to the EcoStruxure Power Commission Online Help.

Click here to download the latest version of EcoStruxure Power Commission software.

Key Features

EcoStruxure Power Commission software performs the following actions for the supported devices and modules:

  • Create projects by device discovery.

  • Save the project in the EcoStruxure Power Commission cloud for reference.

  • Upload standard protection settings to the device and download standard protection settings from the device.

  • Compare the standard protection settings between the project and the device.

  • Generate and print the device standard protection settings report.

  • View the logs and maintenance information.

  • View the alarm details.

  • Check the system firmware compatibility status.

  • Update to the latest device firmware.

  • Perform automatic trip curve tests with preconfigured or custom test points.

  • Perform arc energy reduction tests in compliance with NEC 240.87(C).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.