DOCA0265EN-07

Setting the Instantaneous Overcurrent Protection (I or ANSI 50)

Settings Guideline

Rules for Isd also apply to the Ii threshold.

Application

Principle

Usual value

Secondary side of MV/LV transformer (switchboard main incomer)

Selectivity with downstream circuit breakers

Ii mode: OFF if other MasterPacT MTZ circuit breaker downstream (MicroLogic Active 5.0 and 6.0 only)

Ii = 15 x In if ComPacT NSXm, ComPacT NSX, or PowerPacT P- and R-frame circuit breaker only downstream

Feeder with selectivity with other MasterPacT MTZ, ComPacT NS or PowerPacT P- and R-frame circuit breaker downstream

Same rule as for Isd

Ii mode: OFF (MicroLogic Active 5.0 and 6.0 only)

Feeder without selectivity with other MasterPacT MTZ, ComPacT NS or PowerPacT P- and R-frame circuit breaker downstream

Ii mode: ON

Ii = 10-15 x In

Primary side of LV/LV transformer

Ii mode: OFF (MicroLogic Active 5.0 and 6.0 only)

Generators

Ii mode: OFF (MicroLogic Active 5.0 and 6.0 only)

Power electronic (for example, uninterruptible power supplies, variable speed drives, photovoltaic inverters)

Lower than minimum short-circuit or ground-fault at the end of the protected circuit. Lower setting possible as no selectivity or transient current is expected.

Ii mode: ON

Ii = 2 x In (MicroLogic Active 5.0 and 6.0)

Ii = 1.5 x In (MicroLogic Active 2.0)

Motor

Lower than minimum short-circuit or ground-fault at the end of the cable. Lower setting possible above starting current.

Ii mode: ON

Ii ≥ 13 x Full load current of motor

Ii setting allows normal transient overcurrent inrush current for transformers:

A 1st peak 10 to 25 x In

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.