DOCA0265EN-07

EcoStruxure Power Device App

Presentation

EcoStruxure Power Device app is a single mobile application with the necessary information and capabilities to operate and efficiently maintain devices in the EcoStruxure architecture.

The application enables you to connect to devices, including the following:

  • MasterPacT MTZ circuit breakers

  • TeSys GV4 motor circuit breakers

  • Easergy P3 protection relays

The application can be installed on a smartphone by downloading the application from:

  • Google Play Store for Android smartphones

  • App Store for iOS smartphones

  • iPhone 7 with iOS 13 are the minimum requirements for NFC connectivity.

MasterPacT MTZ Circuit Breakers in EcoStruxure Power Device App

With the EcoStruxure Power Device app, a smartphone can be used with MasterPacT MTZ circuit breakers as the primary interface for day-to-day and critical case maintenance. The MicroLogic Active control unit is identified on the application by scanning the QR code on the device.

EcoStruxure Power Device app is available through:

  • NFC wireless communication (not available with MicroLogic Active 6.0 Ei control unit).

  • USB OTG (On-The-Go) connection.

Using a USB OTG (On-The-Go) Connection

The MicroLogic Active control unit can be powered by an Android smartphone using the USB OTG connection, if necessary.

Using EcoStruxure Power Device app with a USB OTG connection gives access to and allows sharing of the following information types, organized in the following tabs:

  • Quick View: gives an overview of standard protection settings, the health state of the circuit breaker, and recent event history.

  • Protection Setting: displays standard protection settings currently selected, and allows modification of standard protection settings.

For more information, refer to the USB OTG (On-The-Go) connection procedure.

Using an NFC Connection

Connecting to EcoStruxure Power Device app with an NFC connection is always possible, even when the MicroLogic Active control unit is not powered. It gives access to the following information:

  • Information about the MicroLogic Active control unit.

  • Last trip context: trip type; date and time of last trip; current values before trip.

  • Standard and ERMS protection settings (display only).

  • ERMS status.

  • Maintenance:

    • Displays diagnostic counters.

    • Electrical and mechanical operation. Mechanical operation only works if the Control unit is supplied by 24 Vdc.

For more information, refer to the NFC connection procedure.

NOTE: NFC communication is not available with MicroLogic Active 6.0 Ei control unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.