MicroLogic Active Control Unit Identification
Hardware Revision
The hardware revision is an ASCII string using the format AAA.BBB.CCC with:
-
AAA = major version (000 – 127)
-
BBB = minor version (000 – 255)
-
CCC = revision number (000 – 255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2047–0x204C |
8264–8269 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Hardware revision |
Firmware Version
The MicroLogic Active firmware version is available in two formats:
-
For compatibility with MicroLogic X control units, the firmware version is an ASCII string using the format AAA.BBB.CCC, where:
-
AAA = major version (000 – 127)
-
BBB = minor version (000 – 255)
-
CCC = revision number (000 – 255)
The NULL character ends the revision number.
-
-
For compatibility with MicroLogic A/E/P/H trip units, the firmware version is an integer, calculated as follows: AAA*1000 + BBB. For example, 004.002.003 is converted to 4002.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2094–0x2099 |
8341–8346 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Firmware version for compatibility with MicroLogic X control units |
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2005 |
8710 |
R |
1 |
– |
INT16U |
– |
A/E |
Firmware version for compatibility with MicroLogic A/E/P/H trip units |
Product Identification
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x20D9 |
8410 |
R |
1 |
– |
INT16U |
16131–16135 |
A/E |
Product identification : 16131 = MicroLogic Active A 16132 = MicroLogic Active E 16133 = MicroLogic Active AP 16134 = MicroLogic Active 6.0 EP 16135 = MicroLogic Active 6.0 Ei |
|
0x20DA–0x20E3 |
8411–8420 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Vendor name: ‘Schneider Electric’ |
|
0x20E4–0x2123 |
8421–8484 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Vendor URL |
|
0x2124–0x212D |
8485–8492 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Product range: ‘MicroLogic’ |
|
0x212C–0x2132 |
8493–8500 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Product model |
|
0x2134–0x213B |
8501–8508 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Product code |
|
0x213C–0x2148 |
8509–8521 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Serial number of the MicroLogic Active control unit |
|
0x2149–0x2168 |
8522–8553 |
R-WC |
1 |
– |
OCTET STRING |
– |
A/E |
User application name |
|
0x2169–0x2178 |
8554–8569 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Main capability of device |
|
0x2179 |
8570 |
– |
1 |
– |
– |
– |
A/E |
Reserved |
|
0x217A–0x2181 |
8571–8578 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Product range: ‘MasterPacT MTZ’ |
|
0x2182–0x2189 |
8579–8586 |
– |
1 |
– |
– |
– |
A/E |
Reserved |
|
0x218A–0x218D |
8587–8590 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Performance level:
|
|
0x218E–0x219A |
8591–8603 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Serial number of the MasterPacT MTZ circuit breaker |
|
0x219B–0x21AA |
8604–8619 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Device family: ‘Circuit breaker’ |
For compatibility with MicroLogic A/E/P/H trip units, the product identification is also available in registers 8716 and 3816.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x220B |
8716 |
R |
1 |
– |
INT16U |
16131–16135 |
A/E |
Product identification: 16131 = MicroLogic Active A 16132 = MicroLogic Active E 16133 = MicroLogic Active AP 16134 = MicroLogic Active 6.0 EP 16135 = MicroLogic Active 6.0 Ei |
|
0x0EE7 |
3816 |
R |
1 |
– |
INT16U |
16131–16135 |
E |
Product identification with the metering manager: 16132 = MicroLogic Active E 16134 = MicroLogic Active 6.0 EP 16135 = MicroLogic Active 6.0 Ei |
Serial Number
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x21FB–0x21FE |
8700–8703 |
R |
1 |
– |
OCTET STRING |
– |
A/E |
Serial number encoded in ASCII |
Protection Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2223 |
8740 |
R |
1 |
– |
OCTET STRING |
20, 50, 60 |
A/E |
Type of protection:
|
Metering Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2224 |
8741 |
R |
1 |
– |
OCTET STRING |
0x2041, 0x2045 |
A/E |
Type of measurement:
|
Long-Time Protection Activity
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2225 |
8742 |
R |
1 |
– |
INT16U |
1, 10 |
A/E |
Long-time protection activity: 1 = ON 10 = OFF |
Circuit Breaker Type
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2591 |
9618 |
R |
– |
– |
INT16U |
0–2 |
E |
Circuit breaker type: 0 = 3-pole circuit breaker without external neutral current transformer (factory setting) 1 = 4-pole circuit breaker 2 = 3-pole circuit breaker with external neutral current transformer |
Circuit Breaker Characteristics
The characteristics can be downloaded by using the test kit.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x2675 |
9846 |
R |
– |
– |
INT16U |
0–3 |
E |
Standard: 0 = UL 1 = IEC 2 = ANSI 3 = IEC/GB |
|
0x2676 |
9847 |
R |
– |
– |
INT16U |
0 |
E |
Circuit breaker range: 0 = MasterPacT |
|
0x2677–0x267C |
9848–9853 |
R |
– |
– |
OCTET STRING |
– |
E |
Circuit breaker characteristics (for example 'MTZ1 08') |